| Solid Edge Part Type Library : StudyOwner Collection | 
|  AddStudy | Create a new study. | 
|  AddThermalStudy | Create a new Heat Transfer study. | 
|  EditStudyGeom | Edit FEA Study Geometry. | 
|  GetActiveStudy | Get handle to currently active study. | 
|  GetNASTRANScratchDirectoryLocation | Get the location of NASTRAN scratch directory. | 
|  GetSettingsList | Get various settings options from a study owner. | 
|  Item | Get Study From Study Owner. | 
|  SetActiveSetting | Set various settings options on a study owner. | 
|  SetAsmDefaultMaterial | |
|  SetNASTRANScratchDirectoryLocation | Set the location of NASTRAN scratch directory. | 
|  SetStudyActive | Set a specific study as active. Provide study name as input. | 
|  Application | Returns the active application object. | 
|  Count | Returns the number of objects in the referenced collection. | 
|  Parent | Returns the parent object for the referenced object. |