Solid Edge Part Type Library
SetGeometries Method
Description
Set study geometry.
Syntax
Visual Basic
Public Sub SetGeometries( _
   ByRef arrStudyGeomeProxies() As Object _
) 
Parameters
arrStudyGeomeProxies
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objPartDocument As SolidEdgePart.PartDocument = Nothing
        Dim objStudyOwner As SolidEdgePart.StudyOwner = Nothing
        Dim objStudy As SolidEdgePart.Study = Nothing
        Dim objModel As SolidEdgePart.Model = Nothing
        Dim objGeomArray(0) As Object

        Try
            OleMessageFilter.Register()

            ' Connect to Solid Edge
            objApplication = Marshal.GetActiveObject("SolidEdge.Application")
            objPartDocument = objApplication.ActiveDocument

            objStudyOwner = objPartDocument.StudyOwner
            objStudyOwner.GetActiveStudy(objStudy)

            objModel = objPartDocument.Models.Item(1)

            ' Get geometries
            objGeomArray(0) = objModel.Body

            ' Set geometry on study
            objStudy.SetGeometries(objGeomArray)

        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

Study Object  | Study Members  | Solid Edge ST3 - What's New

Send comments on this topic.