Solid Edge Part Type Library
SetNastranOptions Method
Options
Number of modes
Low requency
High Frequency
Command line options
Keyword options
Description
Set various options on NASTRAN solver.
Syntax
Visual Basic
Public Sub SetNastranOptions( _
   ByVal dwOptions As ULong, _
   ByVal ulNumModes As ULong, _
   ByVal dFreqRangeLow As Double, _
   ByVal dFreqRangeHigh As Double, _
   ByVal bstrNasCmdLine As String, _
   ByVal bstrNasKeywordOpts As String _
) 
Parameters
dwOptions
Options
ulNumModes
Number of modes
dFreqRangeLow
Low requency
dFreqRangeHigh
High Frequency
bstrNasCmdLine
Command line options
bstrNasKeywordOpts
Keyword options
Example
Imports System.IO
Imports System.Runtime.InteropServices

Module Example
    <STAThread()> _
    Sub Main()
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objPartDocument As SolidEdgePart.PartDocument = Nothing
        Dim objStudyOwner As SolidEdgePart.StudyOwner = Nothing
        Dim objStudy As SolidEdgePart.Study = Nothing
        Dim dwOptions As UInt32 = 1
        Dim ulNumModes As ULong = 6
        Dim dFreqRangeLow As Double = 1.5
        Dim dFreqRangeHigh As Double = 2.5
        Dim strNasCmdLine As String = "Append=Y"
        Dim strNasKeywordOpts As String = ""

        Try
            OleMessageFilter.Register()

            ' Connect to Solid Edge
            objApplication = Marshal.GetActiveObject("SolidEdge.Application")
            objPartDocument = objApplication.ActiveDocument

            objStudyOwner = objPartDocument.StudyOwner
            objStudyOwner.GetActiveStudy(objStudy)

            objStudy.SetNastranOptions(dwOptions, _
                                       ulNumModes, _
                                       dFreqRangeLow, _
                                       dFreqRangeHigh, _
                                       strNasCmdLine, _
                                       strNasKeywordOpts)

        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
See Also

Study Object  | Study Members  | Solid Edge ST3 - What's New

Send comments on this topic.