|  Application | Returns the active application object. | 
|  AttributeSets | Returns the AttributeSets collection object for the referenced object. | 
|  DisplayName | This read-only String property returns the display name for the referenced object. | 
|  Expose | This read-write Long property sets and returns whether the referenced object is exposed as a custom property.  When set to 1, the object is exposed; when set to 0, the object is not exposed. | 
|  ExposeName | This read-write String property sets and returns the name of the referenced object when the object is exposed as a custom property. | 
|  Formula | Sets and returns the formula of the referenced Variable object. | 
|  IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. | 
|  IsSuppressVariable |  | 
|  Name | Returns the name of the referenced object. | 
|  Parent | Returns the parent object for the referenced object. | 
|  Properties |  | 
|  Suppress | Get and Set of the suppress variable object. | 
|  SystemName | This read-only String property returns the system name for the referenced object. | 
|  Type |  | 
|  UnitsType | Returns the unit type of the referenced Variable object. | 
|  Value | Sets or returns the value of the variable. | 
|  VariableTableName | Returns the name used in the variable table. |