Private Sub Form_Load()
    Dim objApp As SolidEdgeFramework.Application
    Dim objDoc As SolidEdgePart.PartDocument
    Dim objBProfile As SolidEdgePart.Profile
    Dim objBPArray(1 To 2) As SolidEdgePart.Profile
    Dim objModel As SolidEdgePart.Model
    Dim objECProfile As SolidEdgePart.Profile
    Dim objExtCutout As SolidEdgePart.ExtrudedCutout
    Dim objRP As SolidEdgePart.RefPlane
    Dim objEPProfile As SolidEdgePart.Profile
    Dim objExtProt As SolidEdgePart.ExtrudedProtrusion
    Dim objThinWall As SolidEdgePart.Thinwall
    Dim lngStatus As Long
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
        Set objDoc = objApp.Documents.Add("SolidEdge.PartDocument")
        objApp.Visible = True
    Else
        Set objDoc = objApp.ActiveDocument
    End If
    ' *** Create an extruded protrusion as the base feature
    ' Create the profile for the base feature & validate it
    Set objBProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(2))
    Call objBProfile.Circles2d.AddByCenterRadius(x:=0, y:=0, Radius:=0.05)
    lngStatus = objBProfile.End(ValidationCriteria:=igProfileClosed)
    If lngStatus <> 0 Then
        MsgBox "Profile for the base feature is not closed"
    End If
    ' Create the extruded protrusion feature and validate it
    Set objBPArray(1) = objBProfile
    Set objModel = objDoc.Models.AddFiniteExtrudedProtrusion(NumberOfProfiles:=1, ProfileArray:=objBPArray, _
                                                             ProfilePlaneSide:=igSymmetric, ExtrusionDistance:=0.1)
    If (objModel.ExtrudedProtrusions(1).Status <> igFeatureOK) Then
        MsgBox "AddFiniteExtrudedProtrusions method of the Models object fails"
    End If
    objBProfile.Visible = False
    ' *** Create an extruded cutout feature on the base feature
    ' Create the profile for the extruded cutout feature and validate it
    Set objECProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objDoc.RefPlanes(2))
    Call objECProfile.Circles2d.AddByCenterRadius(x:=0, y:=0, Radius:=0.025)
    lngStatus = objECProfile.End(ValidationCriteria:=igProfileClosed)
    If lngStatus <> 0 Then
        MsgBox "Profile for the extruded cutout feature is not closed"
    End If
    ' Create the extruded protrusion feature and validate it
    Set objExtCutout = objModel.ExtrudedCutouts.AddFinite(Profile:=objECProfile, ProfileSide:=igLeft, _
                                                          ProfilePlaneSide:=igRight, Depth:=0.5)
    If (objExtCutout.Status <> igFeatureOK) Then
        MsgBox "AddFinite method of the ExtrudedCutouts object fails"
    End If
    objECProfile.Visible = False
    ' *** Create an extruded protrusion feature on the base feature
    ' Create the profile for the extruded protrusion feature and validate it
    Set objRP = objDoc.RefPlanes.AddParallelByDistance(ParentPlane:=objDoc.RefPlanes(2), Distance:=0.05, NormalSide:=igLeft)
    Set objEPProfile = objDoc.ProfileSets.Add.Profiles.Add(pRefPlaneDisp:=objRP)
    Call objEPProfile.Circles2d.AddByCenterRadius(x:=0, y:=0, Radius:=0.035)
    lngStatus = objEPProfile.End(ValidationCriteria:=igProfileClosed)
    If lngStatus <> 0 Then
        MsgBox "Profile for the extruded protrusion feature is not closed"
    End If
    ' Create the extruded protrusion feature and validate it
    Set objExtProt = objModel.ExtrudedProtrusions.AddFinite(Profile:=objEPProfile, ProfileSide:=igLeft, _
                                                            ProfilePlaneSide:=igLeft, Depth:=0.05)
    If (objExtProt.Status <> igFeatureOK) Then
        MsgBox "AddFinite method of the ExtrudedProtrusions object fails"
    End If
    objEPProfile.Visible = False
    ' *** Create a thin wall feature on the model
    Set objThinWall = objModel.Thinwalls.Add(ThicknessSide:=igInside, CommonThickness:=0.005)
    If (objThinWall.Status <> igFeatureOK) Then
        MsgBox "Add method of thinwall object fails"
    End If
    ' *** Reorder the thin wall feature to place it above the extruded protrusion feature
    Call objThinWall.Reorder(TargetFeature:=objExtCutout, InsertBefore:=False)
    ' USER DISPLAY
    If Not (objDoc.Models(1).Features.Item(3) Is objThinWall) Then
        MsgBox "Reorder method of the ThinWall object fails"
    End If
    ' Release objects
    Set objApp = Nothing
    Set objDoc = Nothing
    Set objBProfile = Nothing
    Set objBPArray(1) = Nothing
    Set objModel = Nothing
    Set objECProfile = Nothing
    Set objExtCutout = Nothing
    Set objRP = Nothing
    Set objEPProfile = Nothing
    Set objExtProt = Nothing
    Set objThinWall = Nothing
End Sub