| Solid Edge Part Type Library : UnitedBody Object | 
|  Delete | Deletes the referenced object. | 
|  DropParents | Removes associative connection with parents, so that it can not edited or recomputed. | 
|  ExactRange | |
|  GetDimensions | |
|  GetSurfaces | |
|  Range | Returns the high and low range values for the referenced object. | 
|  Reorder | Inserts the referenced object in front of or behind another feature. | 
|  RollToFeature | Rolls the referenced Model object back to a specified feature. | 
|  SetSurfaces | 
|  Application | Returns the active application object. | 
|  AttributeSets | Returns the AttributeSets collection object for the referenced object. | 
|  DisplayName | |
|  EdgebarName | |
|  Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. | 
|  Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. | 
|  FacesByRay | Returns a collection of faces that are intersected by a specified vector. | 
|  IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. | 
|  ModelingModeType | |
|  Name | Returns the name of the referenced object. | 
|  Parent | Returns the parent object for the referenced object. | 
|  ShowDimensions | Controls the display of dimensions for the feature object. | 
|  Status | Returns the status of the specified object. | 
|  Suppress | Temporarily suppresses the referenced object. | 
|  SuppressVariable | Returns the suppress variable object. | 
|  SystemName | |
|  Type | Specifies the type of the object being referenced. | 
|  Visible | Specifies whether or not the referenced object is displayed to the screen. |