|  Application | Returns the active application object. | 
|  AttributeSets | Returns the AttributeSets collection object for the referenced object. | 
|  Depth | Sets and returns the distance that the referenced object extends or removes material from a solid. | 
|  DisplayName | This read-only String property returns the display name for the referenced object. | 
|  EdgebarName | This read-only property returns the Edgebar name of the referenced object. | 
|  ExtentSide | Sets and returns the reference plane side for the referenced object. | 
|  ExtentType | Sets and returns the extent type for the referenced object. | 
|  FromPlane | Sets and returns the RefPlane object from which a protrusion, hole, or cutout feature begins. | 
|  GetBottomCapsByModel | Returns a collection of bottom cap faces for the specified model. | 
|  GetEdgesByModel | Returns the edges of a part occurrence specified by the input model. | 
|  GetFacesByModel | Returns the faces of a part occurrence specified by the input model. | 
|  GetFacesByModelAndRay | Returns the faces of a part occurrence specified by the input model and a ray. | 
|  GetSideFacesByModel | Returns a collection of side faces of the weldment feature from the specified model. | 
|  GetTopCapsByModel | Returns a collection of top cap faces of the weldment feature for the specified model. | 
|  IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. | 
|  Name | Returns the name of the referenced object. | 
|  Parent | Returns the parent object for the referenced object. | 
|  ProfileSide | Sets and returns the side of the profile to which material is added or removed. | 
|  ShowDimensions | Controls the display of dimensions for the feature object. | 
|  Status | Returns the status of the specified object. | 
|  Suppress | Temporarily suppresses the referenced object. | 
|  SystemName | This read-only String property returns the system name for the referenced object. | 
|  ToPlane | Sets and returns the RefPlane object from which a protrusion, hole, or cutout feature terminates. | 
|  Type | Specifies the type of the object being referenced. |