Solid Edge Part Type Library
ShowDimensions Property
Collapse All
Expand All
Solid Edge Part Type Library
>
WeldHole Object
: ShowDimensions Property
Description
Controls the display of dimensions for the feature object.
Property type
Read-write property
Syntax
Visual Basic
Public Property ShowDimensions As Boolean
Remarks
If this property is True, the dimensions are displayed; if False, the dimensions are hidden.
See Also
WeldHole Object
|
WeldHole Members
Send comments
on this topic.