|  Application | Returns the active application object. | 
|  AttributeSets | Returns the AttributeSets collection object for the referenced object. | 
|  DisplayName | This read-only String property returns the display name for the referenced object. | 
|  EdgebarName | This read-only property returns the Edgebar name of the referenced object. | 
|  Edges | Returns a collection of edges of a specified type that belong to a model, a feature, or a topology collection of faces. | 
|  Faces | Returns a collection of faces of a specified type that belong to a model, a feature, or a topology object. | 
|  FacesByRay | Returns a collection of faces that are intersected by a specified vector. | 
|  IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. | 
|  Name | Returns the name of the referenced object. | 
|  NumberOfInputFeatures | Returns the number of input features for the referenced pattern. | 
|  NumberOfOccurrences | Returns the number of occurrences of the referenced pattern. | 
|  Parent | Returns the parent object for the referenced object. | 
|  PatternPlane | Returns the PatternPlane object for the referenced object. | 
|  Profile | Sets and returns the Profile object used to construct the referenced feature object. | 
|  ReferenceOccurrence | Sets and returns the pattern occurrence that serves as the reference occurrence. | 
|  ShowDimensions | Controls the display of dimensions for the feature object. | 
|  Status | Returns the status of the specified object. | 
|  Suppress | Temporarily suppresses the referenced object. | 
|  Suppressed | Specifies whether or not the referenced pattern object is suppressed. | 
|  SystemName | This read-only String property returns the system name for the referenced object. | 
|  Transforms | Returns a read-only variant. | 
|  Type | Specifies the type of the object being referenced. |