|  Application | Returns the active application object. | 
|  AttributeSets | Returns the AttributeSets collection object for the referenced object. | 
|  DisplayName | This read-only String property returns the display name for the referenced object. | 
|  EdgebarName | This read-only property returns the Edgebar name of the referenced object. | 
|  EdgeSetCount | Returns the number of edges to which the referenced Round feature applies. | 
|  GetEdgesByModel | Returns the edges of a part occurrence specified by the input model. | 
|  GetFacesByModel | Returns the faces of a part occurrence specified by the input model. | 
|  GetFacesByModelAndRay | Returns the faces of a part occurrence specified by the input model and a ray. | 
|  IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. | 
|  Name | Returns the name of the referenced object. | 
|  Parent | Returns the parent object for the referenced object. | 
|  RadiusType | Returns the radius type for the referenced object. | 
|  ShowDimensions | Controls the display of dimensions for the feature object. | 
|  Status | Returns the status of the specified object. | 
|  Suppress | Temporarily suppresses the referenced object. | 
|  SystemName | This read-only String property returns the system name for the referenced object. | 
|  Type | Specifies the type of the object being referenced. |