|  ActiveSketch | Returns the active Sketch object. | 
|  AddInsStorage | Returns an IUnknown pointer to the object that implements the IStorage corresponding to the add-in substorage for the referenced object. | 
|  Application | Returns the active application object. | 
|  AttachedPropertyTables | Returns the AttachedPropertyTables object for the referenced document object. | 
|  AttributeQuery | Returns the AttributeQuery object. | 
|  CapturedRelationshipCount |  | 
|  ComponentSketches |  | 
|  Constructions | Returns the Constructions collection object. | 
|  CoordinateSystems | Represents a collection of CoordinateSystem objects. | 
|  CreatedVersion | Returns the version of Solid Edge that was used to create the referenced document. | 
|  DesignEdgebarFeatures | This read-only property returns the EdgeBarFeatures collection object (ordered features) for the referenced object.  The collection is dynamically updated, based on history changes. | 
|  DimensionStyles | Returns the DimensionStyles collection object for the referenced document. | 
|  Dirty | Specifies whether or not the referenced document has been modified since the last time it was saved. | 
|  DocumentEvents | Returns the DocumentEvents object for the referenced document object. | 
|  FaceStyles | Returns the FaceStyles collection object for the referenced document. | 
|  FullName | Returns the name and path of the referenced object. | 
|  GeometricVersion | Returns a value that is incremented each time the geometry of an associated document is changed. | 
|  HasCapturedRelationships |  | 
|  HighlightSets | Returns the HighlightSets collection object for the referenced document object. | 
|  HoleDataCollection | Returns the HoleDataCollection object for the referenced document object. | 
|  InPlaceActivated | Specifies whether or not the referenced document is in-place activated. | 
|  InterpartLinks |  | 
|  IsFeatureLibrary | Specifies whether or not the referenced PartDocument or SheetMetalDocument is a feature library. | 
|  IsGeometricVersionDirty | Retrieves whether the geometric version number of the assembly document is dirty or not. | 
|  IsTemplate | Specifies whether or not the referenced document is a template. | 
|  LastSavedVersion | Returns the version of Solid Edge that was used the last time the referenced document was saved. | 
|  Layers | Returns the Layers collection object. | 
|  Name | Returns the name of the referenced object. | 
|  Parent | Returns the parent object for the referenced object. | 
|  Path | Returns the directory path name of the referenced document. | 
|  PhysicalPropertiesStatus | This read-only property returns the status of the physical properties of the model for the referenced object. | 
|  ProfileSets | Returns the ProfileSets collection object for the referenced document object. | 
|  ProfileUndoSteps | This read-write Long property sets and returns the number of profile undo steps for the referenced document object. | 
|  Properties | For document objects, returns the PropertiesCollection colletion object.  For Variables, sets and returns the variable properties. | 
|  PropertyTableDefinitions | Returns the PropertyTableDefinitions object for the referenced document object. | 
|  ReadOnly | Specifies whether or not the referenced document has been opened as read-only. | 
|  RefAxes | Returns the RefAxes collection object for the referenced document object. | 
|  RefPlanes | Returns the RefPlanes collection object for the referenced document object. | 
|  RootStorage | Returns the IUnknown pointer to the object implementing the root storage of the referenced document. | 
|  RoutingSlip | Returns the RoutingSlip object for the referenced document. | 
|  SelectSet | Returns the current selection set for the referenced document. | 
|  Sensors | Returns the Sensors collection object for the referenced document object. | 
|  Sketches | Returns the Sketches collection object for the referenced document object. | 
|  Status | Returns the status of the specified object. | 
|  SummaryInfo | Returns a SheetSummaryInfo object to provide access to descriptive properties for the referenced document. | 
|  Type | Specifies the type of the object being referenced. | 
|  UndoSteps | This read-write Long property sets and returns the number of undo steps for the referenced document object. | 
|  UnitsOfMeasure | Returns the UnitsOfMeasure object for the referenced document. | 
|  Variables | Returns the Variables collection object for the referenced document. | 
|  ViewStyles | Returns the ViewStyles collection object for the referenced document. | 
|  WeldmentModels | Returns the WeldmentModels collection object. | 
|  Windows | Returns the Windows collection object. |