|  Application | Returns the active application object. | 
|  AssemblyWeldments | Returns the AssemblyWeldments collection. | 
|  AttributeSets | Returns the AttributeSets collection object for the referenced object. | 
|  BeadModels | Returns the associated BeadModels object for the referenced WeldmentModel object. | 
|  DisplayCenterOfMass | Controls the display in the assembly of the center-of-mass graphics. | 
|  DisplayCenterOfVolume | Controls the display in the assebmly of the center-of-volume graphics. | 
|  DisplayName | This read-only String property returns the display name for the referenced object. | 
|  DisplayPrincipalAxes | Controls the display in the part of the principal axes graphics. | 
|  Document | Returns the document to which the referenced object belongs. | 
|  EdgebarName | This read-only property returns the Edgebar name of the referenced object. | 
|  Features | Returns the Features collection object for the referenced WeldmentModel. | 
|  FileName | Returns the file name of the referenced document. | 
|  FilletWelds | Returns the FilletWelds collection object. | 
|  GrooveWelds | Returns the GrooveWelds collection object. | 
|  IsAttributeSetPresent | Returns True if a specified Attribute Set exists on the referenced object. | 
|  LabelWelds | Returns the LabelWelds collection object. | 
|  Name | Returns the name of the referenced object. | 
|  Parent | Returns the parent object for the referenced object. | 
|  PartModels | Returns the associated PartModels object for the referenced WeldmentModel object. | 
|  StitchWelds | Returns the StitchWelds collection object. | 
|  SystemName | This read-only String property returns the system name for the referenced object. | 
|  WeldBeadByExtrudedProtrusions | Returns the WeldBeadByExtrudedProtrusions collection object. | 
|  WeldBeadByRevolvedProtrusions | Returns the WeldBeadByRevolvedProtrusions collection object. | 
|  WeldBeadBySweptProtrusions | Returns the WeldBeadBySweptProtrusions collection object. | 
|  WeldChamfers | Returns the WeldChamfers collection object. | 
|  WeldExtrudedCutouts | Returns the WeldExtrudedCutouts collection object. | 
|  WeldHoles | Returns the WeldHoles collection object. | 
|  WeldMirrors | Returns the WeldMirrors collection object. | 
|  WeldPatterns | Returns the WeldPatterns collection object. | 
|  WeldRevolvedCutouts | Returns the WeldRevolvedCutouts collection object. | 
|  WeldRounds | Returns the WeldRounds collection object. |