Solid Edge ST6 SDK
Starting Solid Edge

You may still use the familiar CreateObject() method from the Visual Basic 6 days if you'd like. In Visual Basic .NET, CreateObject() simply calls Activator.CreateInstance. This is important to understand because CreateObject() is a language specific feature of Visual Basic .NET. No other .NET language has a comparable feature. The other .NET languages must rely on Activator.CreateInstance.

See Handling 'Application is Busy' and 'Call was Rejected By Callee' errors for information regarding the use of OleMessageFilter.
Starting Solid Edge from Visual Basic .NET
Copy Code
Imports System.Runtime.InteropServices

Module Program
    <STAThread()> _
    Sub Main()
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objType As Type = Nothing

        Try
            'Old VB6 Syntax
            'objApp = CreateObject("SolidEdge.Application")

            OleMessageFilter.Register()

            ' Get the type from the Solid Edge ProgID
            objType = Type.GetTypeFromProgID("SolidEdge.Application")

            ' Start Solid Edge
            objApplication = Activator.CreateInstance(objType)

            ' Make Solid Edge visible
            objApplication.Visible = True

        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
Starting Solid Edge from C#
Copy Code
using System;
using System.Runtime.InteropServices;

namespace SolidEdge.SDK
{
    class Program
    {
        [STAThread]
        static void Main(string[] args)
        {
            SolidEdgeFramework.Application application = null;
            Type type = null;

            try
            {
                OleMessageFilter.Register();

                // Get the type from the Solid Edge ProgID
                type = Type.GetTypeFromProgID("SolidEdge.Application");

                // Start Solid Edge
                application = (SolidEdgeFramework.Application)
                  Activator.CreateInstance(type);

                // Make Solid Edge visible
                application.Visible = true;
            }
            catch (System.Exception ex)
            {
                Console.WriteLine(ex.Message);
            }
            finally
            {
                OleMessageFilter.Revoke();
            }
        }
    }
}
See Also