Solid Edge ST6 SDK
Units of Measure

        <p>This topic contains these sections:</p>
   
Overview

In the interactive environment, Solid Edge allows you to specify the length, angle, and area units to use when placing, modifying, and measuring geometry. For example, you can specify millimeters as the default length unit of measurement; you can also specify the degree of precision of the readout. You specify these properties on the Units and Advanced Units tabs of the Properties dialog box. (On the File menu, click Properties to display the dialog box.)

This is strictly a manipulation of the display of the precision; internally all measurements are stored at their full precision.

With a Length Readout precision of 0.12, the length of any linear measurement is displayed as follows:

Because millimeters are the default units in this example, whenever distance units are entered, they have to be in millimeters. If a user enters a distance value in inches, for example, the units are automatically converted to millimeters.

 converts to

The units system in Solid Edge allows users to specify the default units and to control how values are displayed for each of the units. Users can change the default units and their display at any time and as often as necessary.

You can customize Solid Edge so that your commands behave in a similar way. For example, suppose you are creating a program to place hexagons. The program displays a dialog box that allows you to enter the size of the hexagon and then creates the hexagon at a location specified by a mouse click. When users enter the size of the hexagon, they should be able to enter the value in the user-specified default unit. Also, users should be able to override the default unit and specify any linear unit. The program will need to handle any valid unit input.

 

Internal Units

Unit Type Internal Units
Distance Meter
Angle Radian
Mass Kilogram
Time Second
Temperature Kelvin
Charge Ampere
Luminous Intensity Candela
Amount of Substance Mole
Solid Angle Steradian

All other units are derived from these. All calculations and geometry placements use these internal units. When values are displayed to the user, the value is converted from the internal unit to the user-specified unit.

When automating Solid Edge, first convert user input to internal units. Calculations and geometric placements use the internal units. When displaying units, you must convert from internal units to default units. The UnitsOfMeasure object handles these conversions.

Working with Units of Measure

The UnitsofMeasure object provides two methods: ParseUnit and FormatUnit. In addition, a set of constants is provided to use as arguments in the methods. The ParseUnit method uses any valid unit string to return the corresponding database units. The FormatUnit method uses a value in database units to return a string in the user-specified unit type, such as igUnitDistance, igUnitAngle, and so forth. The units (meters, inches, and so forth) and precision are controlled by the active units for the document.

The following programs uses both the ParseUnit and FormatUnit methods to duplicate the behavior of unit fields in Solid Edge. The code also checks whether the input is a valid unit key-in and outputs the correctly formatted string according to the user-specified setting.

Error handling is used to determine if a valid unit has been entered. The Text property from the text field is used as input to the ParseUnit method, and the unit is a distance unit. If the ParseUnit method generates an error, focus is returned to the text field, and an error is displayed, giving the user a chance to correct the input. This cycle continues until the user enters a correct unit value. If the key-in is valid, then the database value is converted into a unit string and displayed in the text field.

Formatting and Displaying Units
Formatting and Displaying Units in Visual Basic .NET
Copy Code
Imports SolidEdgeFramework
Imports System.Runtime.InteropServices

Public Class Form1
  Private m_application As SolidEdgeFramework.Application

  Private Sub Form1_Load(ByVal sender As System.Object, _
    ByVal e As System.EventArgs) Handles MyBase.Load

    Try
      ' Connect to a running instance of Solid Edge
      m_application = Marshal.GetActiveObject("SolidEdge.Application")
    Catch ex As Exception
      MessageBox.Show(ex.Message, "Error")
    End Try
  End Sub

  Private Sub Button1_Click(ByVal sender As System.Object, _
    ByVal e As System.EventArgs) Handles Button1.Click
    Dim objDocument As SolidEdgeFramework.SolidEdgeDocument = Nothing
    Dim objUOM As SolidEdgeFramework.UnitsOfMeasure = Nothing
    Dim dHexSize As Double

    Try
      ' Get a reference to the active document
      objDocument = m_application.ActiveDocument

      ' Get a reference to the active document's unit of measure
      objUOM = objDocument.UnitsOfMeasure

      ' Attempt to parse the UOM input by user
      dHexSize = objUOM.ParseUnit( _
        UnitTypeConstants.igUnitDistance, TextBox1.Text)

      ' Update the 2nd textbox with the parsed UOM
      TextBox2.Text = dHexSize.ToString()
    Catch ex As Exception
      MessageBox.Show(ex.Message, "Invalid unit")
    Finally
      If Not (objUOM Is Nothing) Then
        Marshal.ReleaseComObject(objUOM)
        objUOM = Nothing
      End If
      If Not (objDocument Is Nothing) Then
        Marshal.ReleaseComObject(objDocument)
        objDocument = Nothing
      End If
    End Try
  End Sub

  Private Sub Form1_FormClosing(ByVal sender As System.Object, _
    ByVal e As System.Windows.Forms.FormClosingEventArgs) _
    Handles MyBase.FormClosing

    Try
      If Not (m_application Is Nothing) Then
        Marshal.ReleaseComObject(m_application)
        m_application = Nothing
      End If
    Catch ex As Exception
      MessageBox.Show(ex.Message, "Error")
    End Try
  End Sub
End Class
Formatting and Displaying Units in C#
Copy Code
using SolidEdgeFramework;
using System;
using System.Runtime.InteropServices;
using System.Windows.Forms;

namespace Walkthrough
{
    public partial class Form1 : Form
    {
        private SolidEdgeFramework.Application m_application;

        public Form1()
        {
            InitializeComponent();
        }

        private void Form1_Load(object sender, EventArgs e)
        {
            try
            {
                // Connect to a running instance of Solid Edge
                m_application = (SolidEdgeFramework.Application)
                  Marshal.GetActiveObject("SolidEdge.Application");
            }
            catch (System.Exception ex)
            {
                MessageBox.Show(ex.Message, "Error");
            }
        }

        private void Button1_Click(object sender, EventArgs e)
        {
            SolidEdgeFramework.SolidEdgeDocument document = null;
            SolidEdgeFramework.UnitsOfMeasure uom = null;
            double dHexSize = 0;
            try
            {
                // Get a reference to the active document
                document = (SolidEdgeFramework.SolidEdgeDocument)
                  m_application.ActiveDocument;

                // Get a reference to the active document's unit of measure
                uom = document.UnitsOfMeasure;

                // Attempt to parse the UOM input by user
                dHexSize = (double)uom.ParseUnit(
                  (int)UnitTypeConstants.igUnitDistance, TextBox1.Text);

                // Update the 2nd textbox with the parsed UOM
                TextBox2.Text = dHexSize.ToString();
            }
            catch (System.Exception ex)
            {
                MessageBox.Show(ex.Message, "Invalid unit");
            }
            finally
            {
                if (uom != null)
                {
                    Marshal.ReleaseComObject(uom);
                    uom = null;
                }
                if (document != null)
                {
                    Marshal.ReleaseComObject(document);
                    document = null;
                }
            }
        }

        private void Form1_FormClosing(object sender, FormClosingEventArgs e)
        {
            try
            {
                if (m_application != null)
                {
                    Marshal.ReleaseComObject(m_application);
                    m_application = null;
                }
            }
            catch (System.Exception ex)
            {
                MessageBox.Show(ex.Message, "Error");
            }
        }
    }
}
See Also