--------------
Legal Notices
--------------
© 2005, 
UGS Corp.
All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the 
applicable Software License Agreement and contain confidential and proprietary 
information of UGS orp.; which is protected by 
copyright and trade secret law.  Such materials may not be reproduced or 
transferred to other documents or used or disclosed to others for manufacturing 
or for any other purpose except as specifically authorized within the terms of 
the Software License Agreement, or as specifically authorized in writing by 
UGS Corp.
UGS Corp.
5800 Granite Parkway
Suite 600
Plano, TX. 75024
--------------------
End of Legal Notices
--------------------
--------------
Release Notes:
--------------
Product:        Solid Edge
Version:        16.00.04.03
Date:           28-Jan-2005
This release of Solid Edge has been certified to run on the following:
 • Windows 2000 Professional® operating system running Service Pack 4.
 • Windows XP Professional® operating system running Service Pack 1 or 2.
 • Internet Explorer 6.0 or higher
This Update should be installed on top of Solid Edge Version: 
16.00.00.63, 16.00.01.05, 16.00.02.04, 16.00.03.04
--------------------
End of Release Notes
--------------------
------------------------------------
This Update addresses the following:
------------------------------------
=====Assembly=====
PR 1370173: Fixed a crash during assembly file-open.
PR 2043475: Fixed a problem with assembly highlight-related aborts.
PR 5085166: Fixed a crash when Assembly Reports is run and Format button is clicked.
PR 1368331: Fixed a problem where the Frames were not getting deleted properly.
PR 1369165: Fixed a problem where missing holes after edit of ADPF feature 
PR 1373517: Fixed a problem with an inability to delete pipes from the assembly file.
PR 2041609: Fixed a problem with the "As Last Saved" setting on pre-v14 files.
PR 2044976: Fixed a problem with remembering the "As Last Saved" setting in files saved in v15.
PR 5051308: Fixed a problem where modifying end conditions for frames was not working correctly.
PR 5085109: Fixed a problem where system library placement is not listing the connect constraints.
PR 1376701: Fixed a random abort in File-->New experienced with Temp folder being full.
PR 1342142: Fixed a problem where assembly features fail to place correctly when a weldment template is missing.
PR 1370740: Fixed a problem where a crash occurred while editing a tube definition in XpresRoute.
PR 2043463: Fixed a crash in the check interference command.
PR 5117140: Fixes a crash during locate in sketch/profile environment.
PR 1361427: Fixed a problem that was impacting performance of assembly pattern across the network.
PR 2044391: Fixed a problem that will improve display performance.
PR 5101661: Fixed a problem with orientation of texture assignments with rotated textures.
 
=====Part===== 
PR 1365661: Fixed a problem where opening some files was causing Solid Edge to abort.
PR 2039441: Fixed a crash that occurs when applying a round.
PR 5097613: Fixed a crash in the select tool command
PR 5107078: Fixed a crash when entries are deleted from the Save As Flat DXF Options Table
PR 1319482: Fixed a problem causing missing tangent lines in Draft
PR 1346525: Fixes a performance problem with new feature creation.
PR 2041862: Fixed a problem with moving the mouse from the mouse service object after bring up QuickPick.
PR 2043404: Fixed a problem with leaving the starting point of profile plane selected when edited
PR 2043432: Fixed a problem where bead features did not recompute the same when going from V12 to V15
PR 5106457: Fixed a problem where FOP has failed features after recomputing
PR 2044029: Fixed a regression problem during recomputes for loft.
PR 2044153: Fixed a regression problem in dim value change recompute case.
PR 5101680: Fixes a problem with thinfeature recompute.
PR 1375582: Fixed a problem related to Regional setting changes.
PR 5110245: Fixed a problem where Material Thickness was changing when modifying construction Part Copy
=====Draft===== 
 
PR 5080284: Fixed a problem that was causing Solid Edge to abort when importing a dxf file. 
PR 1374593: Fixed a problem with an incomplete SAT data import is fixed
PR 2044405: Fixed a performance problem in VOP wizard when placing multiple views of files that contain tube centerlines.
PR 5096143: Fixed a problem with copying nested groups. 
PR 5082629: Fixed a non-reproducible crash when editing cutting plane line 
PR 5094553: Fixed a problem using edge painter on bend centerlines.
PR 5109963: Fixed a problem saving out to DXF.
PR 5110247: Fixed a problem that lead to an abort with views that contain assembly features.
PR 5112068: Fixed a problem with text font failures when bringing AutoCAD file.
PR 1319482: Fixed a problem with flat pattern missing tangent lines in Draft.
PR 1376349: Fixed a problem where dynamic edit on two sketches at the same time corrupts file.
PR 4913705: Fixed a problem that caused the drawing view shading to not match the VHL very closely.
PR 5038568: Restored function where Hide Edges with fence select selects elements that the fence crosses.
PR 5109263: Fixed a problem where dimensions are losing their style and some of the textboxes are not showing text. 
PR 2044387: Changes have been made to improve display performance. 
 
=====API===== 
PR 2043930: Fixed a problem closing subassemblies via automation.
PR 1357095: Added automation support for Structural Frames
PR 1364773: Added support to obtain the total frame cut length and the individual frame component cut length.
=====Insight=====
PR 5103388: Fixed a problem causing the help about version information to display wrong
PR 1364541: Fixed a problem with pathfinder display after undo checked out after closing without saving
PR 1372335: Fixed a problem where project property Material does get synchronized.
PR 5085032: Fixed a problem where LCA fails to move the large datasets 
PR 5085979: Fixed a problem when overwriting a destination file in LCA the SERevisionRoot is getting the DocID of the original file moved through LCA.
PR 5095693: Fixed a memory leak after dismissing Property Manager dialog.
PR 5103479: Fixed a problem where Rev. Man. doesn't find linked parts in a sub-assembly
PR 5106708: Fixed a problem with the developer logging string for JSPV2_GetAllSites
PR 1331777: Fixed a problem where Insight Connect Properties were not saved with PCF file from Prop Mgr
PR 5096346: Fixed a problem with custom property updates.
PR 1376233: Fixed a problem where file->close command is trying to checkin files which already checked in.
PR 5087371: Fixed a problem where RevMgr is replacing one part for another will not fix links on all Where Used doc.
PR 5117797: Optimized validation of searchscope.txt entries.
PR 5115502: Fixed a problem with Link Resolution Algorithm which is based on common folder '\Insight\'between container path and absolute path.
PR 5108099: Fixed a problem where a few files the Insight Cache says that the file is checked out when the file is actually checked in on the server.
=====MoldTooling===== 
PR 5106452: Fixed a problem to correct a display problem during certain steps in typical MoldTooling workflows.
 
---
End 
---