Solid Edge ST6 SDK
Solid Edge V16 SP7 - Readme

--------------
Legal Notices
--------------
© 2005,
UGS Corp.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of UGS Corp.; which is protected by
copyright and trade secret law.  Such materials may not be reproduced or
transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of
the Software License Agreement, or as specifically authorized in writing by
UGS Corp.

UGS Corp.
5800 Granite Parkway
Suite 600
Plano, TX. 75024

--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        16.00.07.04
Date:           04-May-2005


This release of Solid Edge has been certified to run on the following:
 • Windows 2000 Professional® operating system running Service Pack 4.
 • Windows XP Professional® operating system running Service Pack 1 or 2.
 • Internet Explorer 6.0 or higher


This Update should be installed on top of Solid Edge Version:
16.00.00.63, 16.00.01.05, 16.00.02.04, 16.00.03.04, 16.00.04.03, 16.00.05.02,
16.00.06.03


--------------------
End of Release Notes
--------------------

------------------------------------
This Update addresses the following:
------------------------------------

=====Assembly=====

PR 2047087: Fixed a problem of not being able to create a variable override right after a new member is created.
PR 2047252: Fixed a problem where files are not saved to specified destination when opening an UG assembly.
PR 5053529: Fixed a problem where using QuickPick for Measure was always selecting the first element
PR 1391409: Fixed a problem where interparts would be broken after in-place activating and doing a save as.
PR 5154834: Fixed a problem where IPC fails on an Assembly
PR 1391932: Fixed a problem where Assembly feature failed in V16
PR 1392991: Fixed a problem where relationship on adjustable parts to not update correctly in Move Part.
PR 1394374: Fixed a problem where Pattern of Parts was not updating correctly.
PR 5170963: Fixed a problem where cannot create frame line segments to midpoint

=====Part=====

PR 1390139: Fixed a crash that occurred during display while editing a pattern
PR 5147871: Fixed a crash while displaying sensor status tooltip
PR 2047497: Fixed a problem where density is no longer available in Units properties.
PR 5134998: Fixed a problem with performance opening an assembly file with inactive parts.
PR 5157321: Fixed a case-specific abort
PR 1387673: Fixed a problem in detecting self-intersection during profile validation
PR 5043282: Fixed a problem where control of the unit readout for exposed variable custom properties is now handled through the File Properties->Advanced Units tab except for Density, Accuracy, and Weld Bead Density, which will utilize maximum precision necessary to prevent data loss.
PR 5054338: Fixed a problem protrusion does not use all characters of a Text Profile. Note: In order to see the fix, edit the text by taking one character out and putting it back to trigger a change / update.

=====Draft=====
 
PR 5150756: Fixed a problem where Solid Edge aborts or hangs when text is being placed.
PR 1304193: Fixed a problem with the section view of construction sheets.
PR 1387729: Fixed a problem where coordinates in grid tool are not displayed in older files
PR 1390262: Fixed a problem where parts list balloon quantity is incorrect when opening a draft file without model files
PR 1391507: Fixed a problem with the broken out section view profile shifting after view scale change
PR 5149164: Fixed a problem where 3D dimension gets copied when control dragged
PR 1391787: Fixed a problem with styles on drawing views that have been copied and pasted.
PR 1392388: Fixed a problem where nothing is imported from DWG file using German or Spanish
PR 2047071: Fixed a problem  where you can't drag a center mark in "Draw in View" from one element to another.
PR 1395101: Fixed a problem where sub-assemblies are still included in the parts list with 'exclude reference parts' option selected and all parts of the subassembly are reference parts.

=====API=====

PR 1381448: Quit method in RevisionManager.Application is ready.
PR 5153634: Fixed a problem where modifications to the MechanicalModeling property set now works
PR 1370653: Fixed a problem where an addin menu does not appear in all environments

=====Insight=====

PR 5058274: Fixed a problem where Linked/Embedded Solid Edge files will open quicker.
PR 1391901: Fixed a problem that caused a crash during LCA.
PR 5159362: Fixed a problem where removing access for a doc lib results in no access to other doc libs in that site.
PR 5173623: Fixed an abort while executing the Save command from View and Markup.
PR 1397179: Fixed a problem where you can't view pcf's created from a draft in V16
PR 2049038: Fixed a problem where the Solid Edge Free viewer causes error in inserting image to drawing pcf.

---
End
---