Solid Edge ST6 SDK
Solid Edge V16 SP8 - Readme

--------------
Legal Notices
--------------
© 2005,
UGS Corp.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of UGS Corp.; which is protected by
copyright and trade secret law.  Such materials may not be reproduced or
transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of
the Software License Agreement, or as specifically authorized in writing by
UGS Corp.

UGS Corp.
5800 Granite Parkway
Suite 600
Plano, TX. 75024

--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        16.00.08.02
Date:           10-Jun-2005


This release of Solid Edge has been certified to run on the following:
 • Windows 2000 Professional® operating system running Service Pack 4.
 • Windows XP Professional® operating system running Service Pack 1 or 2.
 • Internet Explorer 6.0 or higher


This Update should be installed on top of Solid Edge Version:
16.00.00.63, 16.00.01.05, 16.00.02.04, 16.00.03.04, 16.00.04.03, 16.00.05.02,
16.00.06.03, 16.00.07.04


--------------------
End of Release Notes
--------------------

------------------------------------
This Update addresses the following:
------------------------------------

=====Assembly=====

PR 5131471: Fixed a problem with in place-deactivate crashing.
PR 1395295: Fixed a problem where Assembly has two parts that do not show in draft or reports.
PR 5167399: Fixed a problem in frames which was causing frames not to update correctly.

=====Part=====

PR 1388943: Fixed a problem where Dynamic edit will now work again on planes that are colinear.
PR 1394695: Fixed a problem of not taking plane input for intersection curves api.
PR 2048356: Fixed a problem where Mass is correctly computed in assembly when 'Show units' option is off in part file.
PR 2048847: Fixed a problem with interoperability between NX and SE
PR 5170406: Fixed a problem with dimension flipping.
PR 5155310: Fixed a case-specific abort when opening part file
PR 1400861: Fixed a problem with renaming multi-hole features so they will now rename their associated variables, as long as the variables have not been named by the user.

=====Draft=====
 
PR 5176538: Fixed a problem where SE aborts when this V12 file is opened
PR 5196160: Fixed a problem where locating a textbox leads to an abort.
PR 2048446: Fixed a problem associated with undoing the creation of the first line in the cutting plane environment.
PR 2049002: Fixed a problem where linear group dimensions on detail views
PR 5172146: Fixed a problem copying and pasting views when a part was not shown in any view.
PR 5179033: Fixed a problem that caused drawing views to fail to update in some workflows
PR 5184516: Fixed a problem where "exclude reference parts" causes sub-assembly's to be excluded from Parts List.
PR 1402037: Fixed a problem where Solid Edge (v16, v17) would crash when opening some pre-v16 .DFT files.
PR 1395118: Fixed a problem translating drawing views to DWG when the specified config is not found.

=====API=====

PR 1359270: Fixed a problem where OLE for DM container is not displaying SE Part in the embedded object site is fixed.

=====Insight=====

PR 1402916: Fixed a problem where SearchScope.txt entries were case sensitive.

---
End
---