| What's New > Solid Edge V16 > Solid Edge V16 SP9 - What's New |
| Item | Description |
|---|---|
| PR 1412431 | Added DrawingView.IsBroken API to indicate if a view is in the broken state. |
| PR 1392663 | Fixed a problem where a macro failed to create interpart constructions. |
| PR 1410684 | Added DrawingView.IsBroken API to indicate if a view is in the broken state. |
| PR 1406741 | UpdateAll automation api updates only the modified documents when debug registry switch UPDATE_ALLMODIFIED_DOCUMENTS is set to 1. |