--------------
Legal Notices
--------------
© 2006, 
UGS Corp.
All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the 
applicable Software License Agreement and contain confidential and proprietary 
information of UGS Corp.; which is protected by 
copyright and trade secret law.  Such materials may not be reproduced or 
transferred to other documents or used or disclosed to others for manufacturing 
or for any other purpose except as specifically authorized within the terms of 
the Software License Agreement, or as specifically authorized in writing by 
UGS Corp.
UGS Corp.
5800 Granite Parkway
Suite 600
Plano, TX. 75024
--------------------
End of Legal Notices
--------------------
--------------
Release Notes:
--------------
Product:        Solid Edge 
Version:        17.00.11.03
Date:           20-Apr-2006
This release of Solid Edge has been certified to run on the following:
 • Windows 2000 Professional® operating system running Service Pack 4.
 • Windows XP Professional® operating system running Service Pack 1 or 2.
 • Internet Explorer 6.0 or higher
This Update can be instaled installed on top of Version: 
17.00.00.65, 17.00.01.06, 17.00.02.04, 17.00.03.04, 17.00.04.03, 17.00.05.03,
17.00.06.03, 17.00.07.03, 17.00.08.03, 17.00.09.03, or 17.00.10.02.
Note: Updates are all inclusive and can be installed on top of the base release
or any released UPdate.
--------------------
End of Release Notes
--------------------
------------------------------------
This Update addresses the following:
------------------------------------
=====Assembly=====
PR 1511090: Fixed a problem where Solid Edge crashes during assembly file-open
PR 1480472: Fixed a problem with an assembly feature
PR 1509025: Fixed a problem where a step translation is missing sub assemblies on export
PR 1509100: Fixed a problem where you are unable to select a part in a subassembly while in-place active
PR 1512311: Fixed a problem where Mirror assembly fails if the template files are read only
PR 2062106: Fixed a problem where you cannot display sketch of other part when editing a part 
PR 2063869: Fixed a problem where Measure minimum distance command does not work properly in IPA'ed sub-asm
PR 2064286: Fixes a problem where Solid Edge crashed in assembly locate.
PR 2065127: Fixed a problem where Solid Edge crashed in the fit command after selecting the "activate" command. 
PR 2063373: Fixed a problem where you can't save a "wrl" file with a name or folder containing double byte characters.
PR 2065402: Fixed a problem with the Inactivate All option when opening assembliess
PR 2064492: Fixed a problem when using Edit Definition on a Part and try to apply any other relationship type besides Mate or Planar Align and it requests you select the part again.
=====Part=====
PR 2063942: Fixed a problem with Select step causes an abort editing a pattern 
PR 5430418: Fixed a non reproducible crash when exiting profile environment
PR 5414713: Fixed a problem with FOP members Material gets reset to parent material if populate
PR 5446562: Fixed a problem where Solid Edge was producing incomplete crashlogs
PR 5442422: Fixed a problem with SetThePixelDust leaks gdi resources.
PR 5445871: Fixed a problem where Solid Edge was producing incomplete crashlogs when running in 3GB
PR 5446096: Improved crashlog data. 
=====Draft=====
PR 1471552: Fixed a problem with FOP variables change from driving to driven.
PR 2063829: Fixed a problem with When the drawing view is updated, the reference element of the dimension is change
PR 2064122: Fixed a problem with If segment is changed with Edge Painter, entire edge changes on update
PR 5360630: Fixed a problem that caused a crash in group dimensions.
PR 5446069: Fixed a problem that caused a crash in group dimensions.
PR 2064302: Fixed a problem where an inserted bitmap object was displaying as dimension color.
 
=====Insight===== 
PR 1500061: Fixed a problem with Bad performance when copying with insight a big assembly.
PR 5393910: Fixed a problem with Family of parts stay released when copied.
---
End 
---