--------------
Legal Notices
--------------
© 2006, 
UGS Corp.
All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the 
applicable Software License Agreement and contain confidential and proprietary 
information of UGS Corp.; which is protected by 
copyright and trade secret law.  Such materials may not be reproduced or 
transferred to other documents or used or disclosed to others for manufacturing 
or for any other purpose except as specifically authorized within the terms of 
the Software License Agreement, or as specifically authorized in writing by 
UGS Corp.
UGS Corp.
5800 Granite Parkway
Suite 600
Plano, TX. 75024
--------------------
End of Legal Notices
--------------------
--------------
Release Notes:
--------------
Product:        Solid Edge 
Version:        17.00.12.01
Date:           12-May-2006
This release of Solid Edge has been certified to run on the following:
 • Windows 2000 Professional® operating system running Service Pack 4.
 • Windows XP Professional® operating system running Service Pack 1 or 2.
 • Internet Explorer 6.0 or higher
This Update can be instaled installed on top of Version: 
17.00.00.65, 17.00.01.06, 17.00.02.04, 17.00.03.04, 17.00.04.03, 17.00.05.03,
17.00.06.03, 17.00.07.03, 17.00.08.03, 17.00.09.03, 17.00.10.02, or 17.00.11.03.
Note: Updates are all inclusive and can be installed on top of the base release
or any released UPdate.
--------------------
End of Release Notes
--------------------
------------------------------------
This Update addresses the following:
------------------------------------
=====Assembly=====
PR 2064989: Fixed a problem where part file could not be saved after using inter-part.
PR 2065979: Fixed a problem where an intersection curve could not be selected when applying a relationship.
PR 5423370: Fixed a problem where an assembly file would not open.
 
=====Part===== 
PR 1510680: Fixed a problem where nothing displayed in a part that contains a Part Copy.
=====Draft=====
PR 1512029: Fixed a problem with Draft file cannot be saved twice.
PR 1506382: Fixed a problem that caused an abort when updating draft quality view with a cutaway
PR 1507747: Fixed a problem where a Hole table update was impossible in V17.
PR 2065677: Fixed a problem that caused an abort when turning on the 'Show' option of view properties.
PR 2065683: Fixed a problem changing "Detail Envelope Properties" with the API
PR 5373067: Fixed a problem where a Draft view become corrupt
---
End 
---