--------------
Legal Notices
--------------
© 2006, 
UGS Corp.
All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the 
applicable Software License Agreement and contain confidential and proprietary 
information of UGS Corp.; which is protected by 
copyright and trade secret law.  Such materials may not be reproduced or 
transferred to other documents or used or disclosed to others for manufacturing 
or for any other purpose except as specifically authorized within the terms of 
the Software License Agreement, or as specifically authorized in writing by 
UGS Corp.
UGS Corp.
5800 Granite Parkway
Suite 600
Plano, TX. 75024
--------------------
End of Legal Notices
--------------------
--------------
Release Notes:
--------------
Product:        Solid Edge 
Version:        17.00.13.01
Date:           16-Jun-2006
This release of Solid Edge has been certified to run on the following:
 • Windows 2000 Professional® operating system running Service Pack 4.
 • Windows XP Professional® operating system running Service Pack 1 or 2.
 • Internet Explorer 6.0 or higher
This Update can be instaled installed on top of Version: 
17.00.00.65, 17.00.01.06, 17.00.02.04, 17.00.03.04, 17.00.04.03, 17.00.05.03,
17.00.06.03, 17.00.07.03, 17.00.08.03, 17.00.09.03, 17.00.10.02, 17.00.11.03,
or 17.00.12.01.
Note: Updates are all inclusive and can be installed on top of the base release
or any released UPdate.
--------------------
End of Release Notes
--------------------
------------------------------------
This Update addresses the following:
------------------------------------
=====Assembly===== 
 
PR 5540685: Fixed a problem with Trap&Rollback - Allowing saving of active doc with no undo logs with SelectTool
PR 1406244: Fixed a problem wherecoordinatesystem based constraints failed
PR 2066585: Fixed a problem where the user is not able to IPA into a part.
PR 5021760: Fixed a problem where it is difficult to locate sketch elements
PR 5526420: Fixed a problem where we were deleting the assembly weldment document when we should not be.
 
=====Part===== 
 
PR 5521270: Fixed a problem that cased Solid Edge to crash when opening large assemblies if all parts are activated
PR 5533331: Fixed a problem that caused a crash following the locate of a tangent surface to define a feature's extent.
PR 2062057: Fixed a problem with incorrect results when deleting faces in this file
PR 2067011: Fixed a problem where Solid edge freezes when the cursor passes over the model. 
 
=====Draft===== 
 
PR 2067514: Fixed a problem that caused an Abort when updating view in this file.
PR 1525448: Fixed a problem where a Draft file fails to open
PR 2066296: Fixed a problem where Dimension tolerance text disappears when selecting two dimensions in a row.
PR 2066379: Fixed a problem where a Draft File cannot be converted into DXF
 
=====Insight===== 
 
PR 2044096: Fixed a problem that caused View & Markup to abort when accessing properties
---
End 
---