| Item |
Description |
| PR 1392663 |
Fixed a problem where a Macro fails to create interpart constructions |
| PR 1406741 |
UpdateAll automation API updates only the modified documents when debug registry switch UPDATE_ALLMODIFIED_DOCUMENTS is set to 1. |
| PR 1410684 |
Fixed a problem where an addin could encounter an invalid argument exception when working with the edgebar. |
| PR 5234060 |
Fixed a problem where the JAsmHideInDrawing occurrence property being incorrectly set. |
| PR 1392422 |
Fixed a problem in automation where inconsistent names are returned by igMouse and DVLines. |
| PR 1412431 |
Added DrawingView.IsBroken API to indicate if a view is in the broken state. |
| PR 1402024 |
Fixed a problem with FOA status property - propauto.dll. |