Solid Edge ST6 SDK
Solid Edge V17 SP6 - Readme

--------------
Legal Notices
--------------
© 2005,
UGS Corp.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of UGS Corp.; which is protected by
copyright and trade secret law.  Such materials may not be reproduced or
transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of
the Software License Agreement, or as specifically authorized in writing by
UGS Corp.

UGS Corp.
5800 Granite Parkway
Suite 600
Plano, TX. 75024

--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        17.00.06.03
Date:           27-Oct-2005


This release of Solid Edge has been certified to run on the following:
 • Windows 2000 Professional® operating system running Service Pack 4.
 • Windows XP Professional® operating system running Service Pack 1 or 2.
 • Internet Explorer 6.0 or higher


This Update should be installed on top of Solid Edge Version:
17.00.00.65, 17.00.01.06, 17.00.02.04, 17.00.03.04, 17.00.04.03, 17.00.05.03


--------------------
End of Release Notes
--------------------

------------------------------------
This Update addresses the following:
------------------------------------

=====Assembly=====

PR 1420619: Fixed a problem where you are unable to pattern after placing an Assembly Feature
PR 1449109: Fixed a problem where an imported ACIS file was generating unusable filenames
PR 2052865: Fixed a problem where the position of an adjustable subassembly changes when opened.
PR 2053523: Fixed a problem where you can not select construction Display button
PR 5306669: Fixed a problem where Parts stay transparent after applying relationships, then can't be hidden.
PR 5325821: Fixed a problem where Parts with # in names lose # and previous characters in Reports.
PR 1449789: Fixed a problem that caused a crash during 'save as image' if coordinate systems are visible
PR 2054556: Fixed a problem that caused an abort when clicking assembly relationship in assembly pathfinder
PR 5332875: Fixed a problem that caused a crash when printing an Assembly file.
PR 2054706: Fixed a problem that caused a crash in JDocument::IOleInPlaceViewsImp::SetActive3DObject.
PR 5332702: Fixed a problem where certain part files would no longer open after an update all and saving an assembly file.
 
=====Part=====

PR 2052480: Fixed a problem where Fujitsu Celsius N430 & J340 crash in command finder.
PR 5223232: Fixed a problem where memory usage goes up as view is rotated if coordinate systems are on.
PR 5321263: Fixed a problem when Display lists have been enable for ATI FireGL graphics cards.
PR 5326203: Fixed a problem with the old ugsplm.com crashlog email address.
PR 5327404: Fixed a problem where you are unable to stitch surfaces imported from NX
PR 2054441: Fixed a problem that could cause an abort based on crashlog data.
PR 5331840: Fixed a problem where a simple part would not flatten after adding flanges.

=====Draft=====

PR 1448552: Fixed a problem with shaded drawing views.
PR 1448976: Fixed a problem where parts in drawing views would show in the wrong position.
PR 5225327: Fixed a problem with embedded Word documents not updating after edit.
PR 5327883: Fixed a problem where File/Open Preview doesn't work with pre-V14 files
PR 5331285: Fixed a problem where attribute text is displaying after translation of DWG file
PR 1449611: Fixed a problem that caused a crash during section view creation

=====API=====

PR 2054505: Fixed a problem where APIs accessing part storage fails.
PR 1446277: Fixed a problem that corrects behavior of AddDraftView automation API.

=====Insight=====

PR 1447004: Improved performance during a window change from ASM to DFT within an Insight environment.

---
End
---