Solid Edge ST6 SDK
Solid Edge V18 SP5 - Readme

--------------
Legal Notices
--------------
© 2006,
UGS Corp.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of UGS Corp.; which is protected by
copyright and trade secret law.  Such materials may not be reproduced or
transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of
the Software License Agreement, or as specifically authorized in writing by
UGS Corp.

UGS Corp.
5800 Granite Parkway
Suite 600
Plano, TX. 75024

--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        18.00.05.05
Date:           27-Apr-2006


This release of Solid Edge has been certified to run on the following:
    • Windows XP Professional® operating system (32-bit) running Service Pack 2
    • Windows XP Professional® operating system (64-bit) running on EM64T hardware
    • Windows 2000 Professional® operating system running Service Pack 4
    • Internet Explorer 6.0 or higher


This Update can be instaled installed on top of Version: 18.00.00.69, 18.00.01.08,
18.00.02.04, 18.00.03.04, or 18.00.04.07.


Note: Updates are all inclusive and can be installed on top of the base release
or any released UPdate.

Note: PR#5434509 was uncovered while preparing to release / post Update 4. A decision
was made to release Update 4 with this known issue. - - PR#5434509: When Hide Previous
Level is enabled, parts cannot be graphically (geometry in the screen) located in a
subassy that has been in-place activated. Workaround: You can locate these parts by;
turning off Hide Previous Level, or locate them in path-finder, or by dragging the
cursor to create a small fence locate. This will be addressed in V18 Update 5.


--------------------
End of Release Notes
--------------------

------------------------------------
This Update addresses the following:
------------------------------------

=====Assembly=====

PR 1511090: Fixed a problem where Solid Edge crashes during assembly file-open
PR 1509100: Fixed a problem where you are unable to select a part in a subassembly while in-place active.
PR 5430943: Fixed a problem where you get in an infinite loop in some doc management events.
PR 1497753: Fixed a problem where Virtual Studio+ displays extra geometry when sharpen is increased
PR 1502278: Fixed a problem where exploded config is not being updated
PR 1504914: Fixed a problem where a Virtual Studio style set in part is not applied in Assembly Virtual Studio+
PR 2063373: Fixed a problem where you can't save a "wrl" file with a name or folder containing double byte characters.
PR 2064286: Fixes a problem where Solid Edge crashed in assembly locate.
PR 2065402: Fixed a problem with the Inactivate All option when opening assemblies.
PR 5404520: Fixed a problem where Assembly pattern is not updating properly when the assembly sketch is modified

=====Part=====

PR 5430418: Fixed a problem where Solid Edge crashed when exiting profile environment
PR 1444929: Fixed a problem where a Sketch Constraint gives unexpected behavior
PR 5301799: Fixed a problem where SMFeatureEdge is not recreating the Flange Profile correctly
PR 1511884: Fixed a problem where a certain part file that contained copy constructions could not be saved.
PR 2065045: Fixed a problem where the Text in view for post processor is incorrect on Japanese Win2000
PR 5217499: Fixed a problem where recalculating a part caused features to fail after loading update 8 for version 16.
PR 5364643: Fixed a problem where Tapered Pipe threads are not created properly – note: existing features that have this problem will need to be recreated.
PR 5446562: Fixed a problem where Solid Edge was creating incomplete crashlogs
PR 5434798: Fixed a problem where Physical Properties Update is not available for Excel driven parts.
PR 5442422: Fixed a problem where SetThePixelDust leaks gdi resources.
PR 5445871: Fixed a problem where Solid Edge was creating incomplete crashlogs when running in 3GB
PR 5446096: Made code changes to improve crashlog data.

=====Draft=====

PR 5417022 / 5395256: Fixed a problem where the Sheet outline does not show after translation
PR 1509225: Fixed a problem with performance when converting a drawing view to 2D.
PR 1510668: Fixed a problem where construction surfaces could not be shown drawing views.
PR 5419923: Fixed a problem where converting a view to 2D dimensions move in some cases.
PR 1471552: Fixed a problem where FOP variables change from driving to driven.
PR 1512366: Fixed a problem where you cannot save a Draft file twice
PR 2063829: Fixed a problem where the reference element of the dimension is changes when updating a drawing view.
PR 5424523: Fixed a problem where Draft files will not open in V18.
PR 5360630: Fixed a problem where Solid Edge crashed with group dimensions.
PR 5446069: Fixed a problem where Solid Edge crashed with group dimensions.
PR 2064302: Fixed a problem where an inserted bitmap object was displaying as dimension color.
PR 5428032: Fixed a problem where a block occurrence is pasted into a document, and the occurrence did now use the block view of the same name.

=====API=====

PR 1450780: Provided a new API GetBendCenterLineAttributesEx() that returns the desired result.

=====Insight=====

PR 5418278: Fixed a problem where managed standard parts are moving while performing LCA.
PR 1508650: Fixed a problem where Revision Manager reports error as SEDocid
PR 5353054: Fixed a problem where you can not do a full text search on draft file.
PR 5393910: Fixed a problem where Family of parts stay released when copied.
PR 5418649: Fixed a problem with cluttered log files
PR 5385256: Fixed a problem where several subassemblies and parts are missing when top level asm is opened
PR 5438065: Fixed a problem where replacing a managed FOA member with a revised version fails in Rev Mgr.
PR 5424012: Fixed a problem where saving a file for the first time is setting the file name to all lower case
PR 5443248: Fixed a problem where you can not open a file with V18
PR 5343986: Fixed a problem where a bogus error was displayed when the option "prevent duplicate filenames" is enabled.


---
End
---