Problem Reports
| Item |
Description |
| PR 5418443 |
Fixed a problem resetting the link resolution property in Revision Manager API. |
| PR 1533978 |
Fixed a problem where a Macro will not change the color of a cutting plane line. |
| PR 1507804 |
Fixed a problem where you are unable to create assembly features using the APIs |
| PR 5556450 |
Enabled Migration commands with a Solid Edge Foundation License |
| PR 2067772 |
Need API for "Subfix 2" of dimension Prefix, added function SubfixString2. |
| PR 2067773 |
Need API for "Subfix horizontal alignment" of dimension Prefix, Added function SubfixAlignment and SubfixAlignmentConstants -
seSubfixAlignLeft and seSubfixAlignCenter |
New APIs
SolidEdgeConstants
SolidEdgeDraft
SolidEdgeFrameworkSupport
See Also