--------------
Legal Notices
--------------
© 2006, 
UGS Corp.
All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the 
applicable Software License Agreement and contain confidential and proprietary 
information of UGS Corp.; which is protected by 
copyright and trade secret law.  Such materials may not be reproduced or 
transferred to other documents or used or disclosed to others for manufacturing 
or for any other purpose except as specifically authorized within the terms of 
the Software License Agreement, or as specifically authorized in writing by 
UGS Corp.
UGS Corp.
5800 Granite Parkway
Suite 600
Plano, TX. 75024
--------------------
End of Legal Notices
--------------------
--------------
Release Notes:
--------------
Product:        Solid Edge 
Version:        19.00.01.06
Date:           27-Sep-2006
This release of Solid Edge has been certified to run on the following:
    • Windows XP Professional® operating system (32 bit or 64 bit) 
    • Internet Explorer 6.0 or higher
This Update can be instaled installed on top of Version: 19.00.00.66.
Note: Updates are all inclusive and can be installed on top of the base release
or any released UPdate.
--------------------
End of Release Notes
--------------------
----------------------------------------------------------
This Update addresses the following Customer Reported PRs:
----------------------------------------------------------
=====Assembly=====
PR 5582013: Fixed a problem where Solid Edge V19 fails to run.
PR 1546531: Fixed a problem where Solid Edge Standard Part fails to run.
PR 5559631: Fixed a problem where Solid Edge crashes when activating parts in this assembly.
PR 5519203: Fixed a problem with Parasolid import performance
PR 5560299: Fixed a problem where move triad does not display in exploded view 
PR 5519203: Fixed a problem with Step file translation performance. Registry files were provided to enable changes.
PR 1541780: Fixed a problem with Round command behavior changed in V19. Radius not keeping last value entered
=====Part=====
PR 5562891: Fixed a problem where deleting a sick relationship causes Solid Edge to abort.
PR 5566826: Fixed a problem where a file crashes with thread textures on
PR 1520837: Fixed a problem where a flat pattern will not update. 
PR 1535616: Fixed a problem where switching between material and gage tabs does retain previous selections.
PR 5373443: Fixed a problem where Dual monitors get multiple min/max/exit buttons on windows, using XP
=====Draft=====
PR 1516308: Fixed a problem where a mirrored block was exported to in the wrong orientation
PR 1536329: Fixed a problem with smart hole depth in hole table.
PR 2068224: Fixed a problem where DXF files can't be imported if Japanese characters are in the file/path name
PR 5395786: Fixed a problem where it is extremely slow saving DXF files to a mapped drive.
PR 1533939: Fixed a problem where SE doesn't import dimensions from file 
PR 5569104: Fixed a problem where Several help .chm files are missing on 2D Drafting (free) CD.
PR 5560331: Fixed a problem where you can't save a drawing to IGES
PR 5586249: Fixed a problem where hatching that is not shown reappears when converting a view to 2D.
=====API=====
PR 5556450: Enabled the Migration commands for a Solid Edge Foundation License
PR 1540237: Fixed a problem with linking against latest version of SEPartReader.zip
PR 1529781: Fixed a problem where StructuralFrame.Get(Set)OverrideEndCondition does not work 
PR 1507804: Fixed a problem adding hole features using the API.
PR 1507804: Fixed a problem with Adding hole features using the API.
=====Insight=====
PR 1534720: Fixed a problem where links can not be resolved after LCA has been used multiple times
PR 2069673: Fixed a problem where the title of a managed document (Insight) found in search would not display
PR 5534235: Fixed a problem where the viewer is not displaying files in a erp system
PR 5566266: Fixed a problem where Solid Edge locked up in attempt to IPA a managed baselined part doc
PR 5567882: Fixed a problem where you cannot place parts from advanced search in parts library
PR 1523670: Fixed a problem where LCA path could not point to a subsite
PR 2070812: Fixed a problem where Cache Manager list box isn't working
PR 5584610: Fixed a problem where Revision Manager does not list the links in this drawing.
PR 5586542: Fixed a problem where PCFs are blank on open.
PR 5589795: Fixed a problem with Difference from V17. Can not choose a site level for the destination
---
End 
---