--------------
Legal Notices
--------------
© 2007, 
UGS Corp.
All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the 
applicable Software License Agreement and contain confidential and proprietary 
information of UGS Corp.; which is protected by 
copyright and trade secret law.  Such materials may not be reproduced or 
transferred to other documents or used or disclosed to others for manufacturing 
or for any other purpose except as specifically authorized within the terms of 
the Software License Agreement, or as specifically authorized in writing by 
UGS Corp.
UGS Corp.
5800 Granite Parkway
Suite 600
Plano, TX. 75024
--------------------
End of Legal Notices
--------------------
--------------
Release Notes:
--------------
Product:        Solid Edge 
Version:        19.00.10.04
Date:           19-Oct-2007
This release of Solid Edge has been certified to run on the following:
    • Windows XP Professional® operating system (32 bit or 64 bit) 
    • Internet Explorer 6.0 or higher
This Update can be instaled installed on top of Version: 19.00.00.66, 19.00.01.06,
19.00.02.06, 19.00.03.06, 19.00.04.06, 19.00.05.03, 19.00.06.04, 19.00.07.03, 
19.00.08.04, or 19.00.09.03.
Note: Updates are all inclusive and can be installed on top of the base release
or any released UPdate.
--------------------
End of Release Notes
--------------------
-------------------
Installation Notes:
-------------------
After downloading the Update to your machine, dbl click the downloaded file
and the Update will install.
-------------------
End of Installation
-------------------
----------------------------------------------------------
This Update addresses the following Customer Reported PRs:
----------------------------------------------------------
=====Assembly=====
PR 2085656: Fixed a problem a crash based on info received in a auto-capture crashlog
PR 5792725: Fixed a problem that caused a crash in Assembly.
PR 2085774: Fixed a problem where you cannot save this file to JT in V19
PR 2084868: Fixed a problem were the cursor leaves trails and zingers
PR 2088108: Fixed a problem where Physical Props are not reporting unassigned densities correctly.
PR 1580928: Fixed a problem positioning hole assembly features.
PR 1616060: Fixed a problem where a Parasolid asm file fails to import
PR 5588898: Fixed a problem where a section view is causing file size increase after a save.
PR 2088423: Fixed a problem where the assembly ribbon bar is flickering during Close & Return to an expanded asm.
=====Part=====
PR 5811217: Fixed a problem where resizing ref planes gives wrong member geometry
PR 2088201: Fixed a problem where the cursor jumps when reordering the feature
PR 2088098: Fixed a problem that caused a crash when executing "GO TO" command
PR 5798598: Fixed a problem where Lightworks Framework Application failed while launching Material Table
PR 2089001: Fixed a problem where editing a cutout profile and finishing without changes results in a recompute
PR 5822624: Fixed a problem where you are unable to get a contour flange around an internal octagon at desired angle
=====Draft=====
PR 1617165: Fixed a problem where sheets are missing in an exported DXF file.
=====Insight=====
PR 5806293: Fixed a problem where RevMan deletes part file if files are renamed to the same name.
PR 1607695: Fixed a problem where Redefine links does not work
PR 2086755: Fixed a problem where Japanese file names are garbled in View & Markup
PR 2060477: Fixed a problem where you cannot save a Solid Edge file using Japanese name as PCF.
PR 5832513: Added an Obsolete option in the function "Move documents through workflow"
---
End 
---