--------------
Legal Notices
--------------
© 2007, 
UGS Corp.
All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the 
applicable Software License Agreement and contain confidential and proprietary 
information of UGS Corp.; which is protected by 
copyright and trade secret law.  Such materials may not be reproduced or 
transferred to other documents or used or disclosed to others for manufacturing 
or for any other purpose except as specifically authorized within the terms of 
the Software License Agreement, or as specifically authorized in writing by 
UGS Corp.
UGS Corp.
5800 Granite Parkway
Suite 600
Plano, TX. 75024
--------------------
End of Legal Notices
--------------------
--------------
Release Notes:
--------------
Product:        Solid Edge 
Version:        19.00.03.06
Date:           18-Jan-2007
This release of Solid Edge has been certified to run on the following:
    • Windows XP Professional® operating system (32 bit or 64 bit) 
    • Internet Explorer 6.0 or higher
This Update can be instaled installed on top of Version: 19.00.00.66, 19.00.01.06, 
or 19.00.02.06.
Note: Updates are all inclusive and can be installed on top of the base release
or any released UPdate.
--------------------
End of Release Notes
--------------------
----------------------------------------------------------
This Update addresses the following Customer Reported PRs:
----------------------------------------------------------
=====Assembly=====
PR 1550966: Fixed a problem where Standard Parts does not create selected part
PR 5532555: Fixed a problem where Sub-Assembly display configurations cause all parts to be hidden.
PR 5608103: Fixed a problem where automatic frame component positioning does not work 
PR 5631004: Fixed a problem where section view FF show lines and a circle that should not be there. 
PR 2073663: Fixed a problem where the Position3d constraint fails to move part after modifying sketch that drives it
PR 5656020: Fixed a problem where Section Views in assembly are not cutting parts properly for symmetric through-all
PR 5657836: Fixed a problem where you can't place variable length standard parts after installing update 2.
PR 5648138: Fixed a problem with the default output folder path when opening a UG file
PR 5656912: Fixed a problem where Solid Edge crashes when creating an assembly pattern
PR 1531552: Fixed a problem where a CAM relationship creates interference between parts.
PR 1557045: Fixed a problem with performance in assembly
PR 1564217: Fixed a problem where clicking on a triad origin dismisses triad while placing dimension.
PR 5624749: Fixed a problem where the STL translator is not trimming surfaces correctly.
PR 1545313: Fixed a problem where editing a section view is not possible in Design & Drafting and Solid Edge Foundation
PR 5660221: Fixed a problem where an IGES file translation results in missing parts.
=====Part=====
PR 5624183: Fixed a problem where changing the BlueSurf option to Tangent causes Solid Edge to crash
PR 1560496: Fixed a problem with STEP files that were created with a comma as the decimal delimiter
PR 5582087: Fixed a problem where you are "Unable to create body" using mirror sketch curves to create Dimple 
PR 5610135: Fixed a problem where Undo results are incorrect after making profile changes in Part.
PR 5660666: Fixed a problem where print from wireframe mode in Profile does not include profile geometry. 
PR 5660770: Fixed a problem where the 2nd horizontal chained dimension gets placed incorrectly
PR 5669631: Fixed a problem where Solid Edge crashed after recomputing a Flat Patten
PR 2066862: Added a tool that allows links to non-existent FOP and divide part member files to be removed. 
PR 5677117: Fixed a problem where Move Face with keyin and Return terminates the command.
PR 5683208: Fixed a problem with When a attempt to convert using SEPROE.exe a license error occurs. 
=====Draft=====
PR 5633556: Fixed a problem where a Parts list would not stay up to date. 
PR 5618414: Fixed a problem where old DQ views were updating incorrectly.
PR 1554625: Fixed a problem where a Draft file opens in V16 and V17, but not in V18 or V19
PR 1557190: Fixed a problem where complex strings are not displaying in block occurrences.
PR 5659161: Fixed a problem where Update 2 scales dimensions to the views scale on export to DXF
PR 5593722: Fixed a problem where copy and paste title block results in wrong size text/lines
PR 1560113: Fixed a problem where you are unable to open this DXF file in V19
PR 2075329: Fixed a problem where the display of a weld reinforcement symbol is not correct
PR 5650136: Fixed a problem where a DXF file created by Solid Edge cannot be opened in AutoCAD
PR 5666550: Fixed a problem where Copy and Paste changes text fonts
PR 5671002: Fixed a problem where the GDT font aspect ratio is not set to 1 when opening an AutoCAD file
PR 5657881: Fixed a problem where Solid Edge crashes when placing a distance between dimension
=====API=====
PR 1553359: Fixed a problem with Frames API
PR 1553510: Fixed a problem with GetOrientation for StructuralFrame
PR 5389793: Fixed a problem where an application's locale changing when loading separtreader.dll. 
=====Insight=====
PR 1551714: Fixed a problem where performance on file open very slow in V18 Update 8 compared to V16 Update 9.
PR 1557352: Fixed a problem where ServerMap.txt doesn't work - Insight still tries to access the old server
PR 1560300: Fixed a problem where LCA Dialog doesn't update the file list for the SharePoint doclib folder
PR 5613700: Fixed a problem where Solid Edge search will not search document libraries in sub sites
PR 5648569: Fixed a problem where you cannot open and revise on the fly from internet explorer dashboard
PR 5651802: Fixed a problem where Create in Place command fails when using a FQDN naming convention for the URL.
PR 1554819: Fixed a problem where validating searchscope entries takes approx. 20 seconds.
PR 5660196: Fixed a problem with performance when searching large number of doclibs
PR 1562958: Fixed a problem where search doesn't return a result when the user doesn't have access to a document library
PR 1563289: Fixed a problem where a search never ends when "Look in" the top level site is specified
PR 5613700: Fixed a problem where Solid Edge search will not search document libraries in sub sites
PR 5659034: Fixed a problem where the File Open dialog does not remember the last used folder.
PR 5670057: Fixed a problem where 50 or so files were deleted from server and local cache
---
End 
---