--------------
Legal Notices
--------------
© 2007, 
UGS Corp.
All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the 
applicable Software License Agreement and contain confidential and proprietary 
information of UGS Corp.; which is protected by 
copyright and trade secret law.  Such materials may not be reproduced or 
transferred to other documents or used or disclosed to others for manufacturing 
or for any other purpose except as specifically authorized within the terms of 
the Software License Agreement, or as specifically authorized in writing by 
UGS Corp.
UGS Corp.
5800 Granite Parkway
Suite 600
Plano, TX. 75024
--------------------
End of Legal Notices
--------------------
--------------
Release Notes:
--------------
Product:        Solid Edge 
Version:        19.00.05.03
Date:           19-Apr-2007
This release of Solid Edge has been certified to run on the following:
    • Windows XP Professional® operating system (32 bit or 64 bit) 
    • Internet Explorer 6.0 or higher
This Update can be instaled installed on top of Version: 19.00.00.66, 19.00.01.06,
19.00.02.06, 19.00.03.06, or 19.00.04.06.
Note: Updates are all inclusive and can be installed on top of the base release
or any released UPdate.
--------------------
End of Release Notes
--------------------
----------------------------------------------------------
This Update addresses the following Customer Reported PRs:
----------------------------------------------------------
=====Assembly=====
PR 1581284: Fixed a problem where a message was not displayed when a SaveAs failed on a write-protected part.
PR 1582000: Fixed a problem where simplified assembly display is clipped
PR 1583107: Fixed a problem where changes made to a sketch were lost after saving assembly
PR 2076006: Fixed a problem with the creation of physical conductors.
PR 5619983: Fixed a problem where assembly parts were getting ?'s in pathfinder indicating missing components.
PR 5687761: Fixed a problem where Property Text gives bad data for simplified assemblies in PMI.
PR 5703102: Fixed a problem where changes made in Edit Table are not retained
PR 5663102: Fixed a problem where a strange circle displays in this drawing view
PR 5715979: Fixed a problem where Solid Edge displays a "Solid Edge requires additional memory to... " error
PR 1533732: Fixed a problem where Assembly pattern positions parts incorrectly
PR 5665884: Fixed a problem where Assembly hangs replacing a part
PR 5683521: Fixed a problem where you cannot replace an alternate sub-assembly.
PR 5600044: Fixed a problem where parts are going over constrained after creating a new FOA member using the table editor
=====Part=====
PR 1580247: Fixed a problem where Solid Edge crashes when normal cutout is used for a logo
PR 2078811: Fixed a problem where "Bend relief" is not correctly displayed.
PR 5709603: Fixed a problem where the Family Identifier message when editing threaded holes is misleading
PR 5218427: Fixed a problem where you cannot edit text profile when anchored to an arc
=====Draft=====
PR 1582140: Fixed a problem where Solid Edge aborts when clicking on the Options button when exporting to DWG
PR 1545609: Fixed a problem where image from a draft file are removed when saved.
PR 1583952: Fixed a problem with thread display at chamfer
PR 5524235: Fixed a problem where clip art pasted from word is displaying incorrectly.
PR 5681877: Fixed a problem where 3D DWG files do not import as SAT from ACAD 2004
PR 5722213: Fixed a problem where incorrect dimension values show in acad when a draft is exported
PR 1583575: Fixed a problem where saving a DWG or DXF in TEMP folder produces an error
PR 1586550: Fixed a problem where brackets of a reference dimension will be printed in a lighter color.
PR 1586577: Fixed a problem where Solid Edge V19 Update 4 imports the AutoCAD Color 7 as white
PR 2080071: Fixed a problem where imported line styles from DWG incorrect.
PR 2080212: Fixed a problem where linear dimensions export with no picture data
=====API=====
PR 1573535: Fixed a problem with threads in API in a C# program
 
=====Insight===== 
PR 1563966: Fixed a problem where Search functionality is not working correctly when the user searches on a Property
PR 1579038: Fixed a problem where the checked out cfg files cannot be checked in
PR 2079055: Fixed a problem where 'Part Name' Japanese strings are garbled in Pathfinder
PR 5710686: Fixed a problem where Long File names are not displayed completely on Solid Edge close dialog
PR 5357907: Fixed a problem where the Revision command was not handling an FOA revision correctly
PR 5726666: Fixed a problem where FOP Master file is crashing in Rev Manager when renaming
---
End 
---