--------------
Legal Notices
--------------
©2008 Siemens Product Lifecycle Management Software Inc.
All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the 
applicable Software License Agreement and contain confidential and proprietary 
information of Siemens Product Lifecycle Management Software Inc.; which is 
protected by copyright and trade secret law. Such materials may not be reproduced 
or transferred to other documents or used or disclosed to others for manufacturing 
or for any other purpose except as specifically authorized within the terms of the 
Software License Agreement, or as specifically authorized in writing by Siemens 
Product Lifecycle Management Software Inc.
Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024
--------------------
End of Legal Notices
--------------------
--------------
Release Notes:
--------------
Product:        Solid Edge 
Version:        20.00.10.03
Date:           24-Oct-2008
This release of Solid Edge has been certified to run on the following:
    • Windows XP Professional® operating system (32 bit or 64 bit) 
    • Windows Vista Business® or Vista Enterprise® operating system (32 bit or 64 bit) 
    • Internet Explorer 7.0 (IE 6.0 minimum) 
This Update can be installed on top of Version: 
20.00.00.96, 20.00.01.08, 20.00.02.03, 20.00.03.03, 20.00.04.04, 20.00.05.05, 
20.00.06.06, 20.00.07.04, 20.00.08.04, or 20.00.09.03.
Note: Updates are all inclusive and can be installed on top of the base release
      or any released Update.
--------------------
End of Release Notes
--------------------
-------------------
Installation Notes:
-------------------
After downloading the Update to your machine, dbl click the downloaded file
and the Update will install.
-------------------
End of Installation
-------------------
----------------------------------------------------------
This Update addresses the following Customer Reported PRs:
----------------------------------------------------------
=====Assembly=====
PR 5737340: Fixed a problem that caused a circular dependency error using FlashFit.
PR 1649779: Fixed a problem where the DELETE key in assembly does not work at times.
PR 2076104: Fixed a problem where in the user is unable to auto-restore a backed up file.
PR 1628066: Fixed a problem with FOA and Assembly Features
PR 2088091: Fixed a problem where it takes too much time and memory to update the "Physical Properties”
PR 2085635: Fixed an abort from data submitted via a crashlog.
PR 6022024: Fixed a problem with include that was introduced in Update 9.
PR 1681255: Fixed a problem where Save As Image does not create a rendered image in Foundation 
PR 1586883: Fixed a problem where Part colors are not exported to step.
PR 6023710: Fixed a problem where washers are not available with C'snk screw 
PR 6001319: Fixed a problem where embedded weldment information gets lost
PR 6026967: Fixed a problem where previous custom part inherits length of the most recently placed part.
PR 6033504: Fixed a problem where a revolved cutout is removing material where there is no sketch.
PR 6000242: Fixed a problem where you are unable to import an STL file. 
=====Part=====
PR 6006751: Fixed a problem where the Hole Table is not listing the correct hole diameters for a counterbore
PR 1641087: Fixed a problem that was causing a crash with an old part in V20 SP3
PR 1668197: Fixed a problem where DIN.PZL will not be used for lofted flanges
PR 1680457: Fixed a problem where typing "=" and selecting dim adds multiple entries to variable table. 
PR 5782978: Fixed a problem where moving the cursor over Variable table causes zoom to happen or automatically
PR 2105606: Fixed a problem where a Round disappears when part is recomputed in Version 20 
PR 2102531: Fixed a problem where creating an open profile protrusion on a tapered face failed in V20
PR 2096263: Fixed a problem where you are unable to make a dimple that uses an inside edge.
PR 1603406: Fixed a problem with mirror performance on grouped 2D elements, maintain relationships on 
PR 6040150: Fixed a problem with Tool Tips not displaying properly when using SmarTeam
=====Draft=====
PR 5992242: Fixed a problem where EMF's are scaled incorrectly 
PR 5941495: Fixed a problem where a specific workflow with Blocks will cause a draft file to be unusable. 
PR 5969985: Fixed an abort from data submitted via a crashlog.
PR 2107915: Fixed a problem where data alignment in table properties is incorrect
PR 6024647: Fixed a problem that caused Solid Edge to crash when copying a fill style
PR 2105954: Fixed a problem where a Japanese font is not mapped to an ACAD font. 
PR 1684163: Fixed a problem where you cannot copy and paste a view that contains a coordinate dim
PR 1535069: Fixed a problem where you are unable to hide an overridden edge segment 
PR 6031576: Fixed a problem where Solid Edge runs out of memory when working with shading Drawing views.
PR 1644606: Fixed a problem where a drawing view is never up to date
PR 1632537: Fixed a problem where you save a Solid Edge draft file as a pdf file and the output is rotated. 
PR 6020990: Fixed a problem where you cannot import a draft file
=====API===== 
 
PR 5544696: Fixed a problem with Expose Parasolid id/tag via API for Body, Edge, Face, Loop, Shell and Vertex
PR 1619947: Fixed a problem with a call to SurfaceBoundaries.Add failing with 'type mismatch'.
=====Insight/===== 
 
PR 5549874: Fixed a problem where Parts are shown as Designed even though they are Simplified parts
PR 6029411: Fixed a problem where Solid Edge crashed when IPA on a part or assembly from a checked out Draft file.
---
End 
---