--------------
Legal Notices
--------------
©2009 Siemens Product Lifecycle Management Software Inc.
All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the 
applicable Software License Agreement and contain confidential and proprietary 
information of Siemens Product Lifecycle Management Software Inc.; which is 
protected by copyright and trade secret law. Such materials may not be reproduced 
or transferred to other documents or used or disclosed to others for manufacturing 
or for any other purpose except as specifically authorized within the terms of the 
Software License Agreement, or as specifically authorized in writing by Siemens 
Product Lifecycle Management Software Inc.
Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024
--------------------
End of Legal Notices
--------------------
--------------
Release Notes:
--------------
Product:        Solid Edge 
Version:        20.00.13.04
Date:           20-Mar-2009
This Update can be installed on top of Versions: 
20.00.00.96, 20.00.01.08, 20.00.02.03, 20.00.03.03, 20.00.04.04, 20.00.05.05, 
20.00.06.06, 20.00.07.04, 20.00.08.04, 20.00.09.03, 20.00.10.03, 20.00.11.06,
20.00.12.02.
Note: Updates are all inclusive and can be installed on top of the base release
      or any released Update.
--------------------
End of Release Notes
--------------------
-------------------
Installation Notes:
-------------------
After downloading the Update to your machine, dbl click the downloaded file
and the Update will install.
-------------------
End of Installation
-------------------
----------------------------------------------------------
This Update addresses the following Customer Reported PRs:
----------------------------------------------------------
=====Assembly=====
PR 6088990: Assembly feature performance 
PR 6100668: Printing an assembly sketch causes Solid Edge to crash
PR 6097501: Weld features failed each time the weldment asm is opened
PR 6087130: Improvements to assembly feature performance on open/show
=====Part=====
PR 1601288: View of PMI with Insight Connect with unit "Millimeter"
PR 1698243: Image component not found in foundation license
PR 5957757: Break corner fails for this specific case
PR 6012839: Simplification of flat pattern was not handled in many cases
=====Draft=====
PR 5858671: Added registry based "Print As Black" option to Save As PDF
PR 2116184: Product aborts when changing dimension style options
PR 6107739: Unable to see fence with AutoCAD color scheme
PR 2112299: Cannot create the 'Section Only' with PMI model view
PR 6107872: Annotations do not show in JT model views
===API===
PR 1628650: Automation workflow causes file properties to be deleted
---
End 
---