Solid Edge ST6 SDK
Solid Edge V20 SP2 - Readme

--------------
Legal Notices
--------------
© 2007,
UGS Corp.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of UGS Corp.; which is protected by
copyright and trade secret law.  Such materials may not be reproduced or
transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of
the Software License Agreement, or as specifically authorized in writing by
UGS Corp.

UGS Corp.
5800 Granite Parkway
Suite 600
Plano, TX. 75024

--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        20.00.02.03
Date:           19-Nov-2007

This release of Solid Edge has been certified to run on the following:
    • Windows XP Professional® operating system (32 bit or 64 bit)
    • Windows Vista Business® or Vista Enterprise® operating system (32 bit or 64 bit)
    • Internet Explorer 7.0 (IE 6.0 minimum)

This Update can be instaled installed on top of Version: 20.00.00.96, or 20.00.01.08.

Note: Updates are all inclusive and can be installed on top of the base release
      or any released UPdate.

--------------------
End of Release Notes
--------------------

-------------------
Installation Notes:
-------------------

After downloading the Update to your machine, dbl click the downloaded file
and the Update will install.

-------------------
End of Installation
-------------------

----------------------------------------------------------
This Update addresses the following Customer Reported PRs:
----------------------------------------------------------

=====Assembly=====

PR 5827283: Fixed a problem where Explode Config used for ERA goes bad after adding a motor and entering animation
PR 2088108: Fixed a problem where Physical Props are not reporting unassigned densities correctly selected parts.
PR 1580928: Fixed a problem with the positioning of hole assembly feature.
PR 5588898: Fixed a problem where a section view is causing file size increase after a save.
PR 2088423: Fixed a problem where the assembly ribbon flickering when user is Closing & Returning to an expanded asm.
PR 1609662: Fixed a problem where the user is unable to delete pipe occurrences.
PR 5815906: Fixed a problem where Solid Edge is crashing when you try to save out an empty simplified assembly.
PR 2083366: Fixed a problem where Section cut faces are not updating properly.
PR 5828903: Fixed a problem where you can not select a silhouette edge of one part.
PR 5765837: Fixed a problem where Export to JT did not honor Solid Edge Occurrence Properties
PR 1579648: Fixed a problem where entries from custom.xml are not used and cannot be deleted
PR 5831498: Fixed a problem with assembly file-open performance

=====Part=====

PR 2089001: Fixed a problem where editing a cutout profile and finishing without changes results in a recompute
PR 5822624: Fixed a problem where you are unable to get a contour flange around an internal octagon
PR 5747437: Fixed a problem where a symmetry relationship not be created
PR 1624643: Fixed a problem where German Locale shows read/write fields incorrectly in variable table

=====Draft=====

PR 1617165: Fixed a problem where sheets are missing when using Save as DXF
PR 5822573: Fixed a problem where you are unable to Copy/Move multiple elements in Draw in View.
PR 5827506: Fixed a problem where this Draft file does not open.
PR 5831180: Fixed a problem where you are unable to create a PDF dataset.
PR 5835355: Fixed a problem where this Draft file does not open.
PR 1619145: Fixed a problem where bend table column headers are not displayed.
PR 5622219: Fixed a problem where dangling dimension have the wrong value when reattached

=====Insight=====

PR 5832513: Fixed a problem where there was no Obsolete option in the function "Move documents through workflow"
PR 5831605: Fixed a problem where you are unable to display a pcf file in the View and Markup environment.

---
End
---