Solid Edge ST6 SDK
Solid Edge V20 SP3 - Readme

--------------
Legal Notices
--------------
© 2007,
UGS Corp.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of UGS Corp.; which is protected by
copyright and trade secret law.  Such materials may not be reproduced or
transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of
the Software License Agreement, or as specifically authorized in writing by
UGS Corp.

UGS Corp.
5800 Granite Parkway
Suite 600
Plano, TX. 75024

--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        20.00.03.03
Date:           12-Dec-2007

This release of Solid Edge has been certified to run on the following:
    • Windows XP Professional® operating system (32 bit or 64 bit)
    • Windows Vista Business® or Vista Enterprise® operating system (32 bit or 64 bit)
    • Internet Explorer 7.0 (IE 6.0 minimum)

This Update can be instaled installed on top of Version: 20.00.00.96, 20.00.01.08, or
20.00.02.03.

Note: Updates are all inclusive and can be installed on top of the base release
      or any released UPdate.

--------------------
End of Release Notes
--------------------

-------------------
Installation Notes:
-------------------

After downloading the Update to your machine, dbl click the downloaded file
and the Update will install.

-------------------
End of Installation
-------------------

----------------------------------------------------------
This Update addresses the following Customer Reported PRs:
----------------------------------------------------------

=====Assembly=====

PR 1619968: Fixed a problem where assembly files would not open.
PR 1605721: Fixed a problem where a Fastener System cannot be deleted
PR 5858754: Fixed a problem that caused Solid Edge to crash based on submitted crashlogs
PR 1622291: Fixed a problem where native STEP file import is missing sub asm names

=====Part=====

PR 2089934: Fixed a problem where Solid Edge fails to execute in a timely manner using a License File list.
PR 1623107: Fixed a problem with Wrong result in flatten in V19

=====Draft=====

PR 5849264: Fixed a problem where the "last printed date" property is not updating before printing.
PR 1625754: Fixed a problem where Solid Edge is crashing while zooming in and out of filled box in draft
PR 1625692: Fixed a problem where Hebrew text in PMI callout is reversed [ABCD=DCBA]
PR 1624209: Fixed a problem where 64bit Solid Edge crashes when updating drawing views.
PR 5841792: Fixed a problem where Parts List and Auto ballooning is not updating properly.
PR 1627832: Fixed a problem where the submitted Draft file aborts on open.

---
End
---