--------------
Legal Notices
--------------
© 2007,
UGS Corp.
All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of UGS Corp.; which is protected by
copyright and trade secret law. Such materials may not be reproduced or
transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of
the Software License Agreement, or as specifically authorized in writing by
UGS Corp.
UGS Corp.
5800 Granite Parkway
Suite 600
Plano, TX. 75024
--------------------
End of Legal Notices
--------------------
--------------
Release Notes:
--------------
Product: Solid Edge
Version: 20.00.04.04
Date: 24-Jan-2008
This release of Solid Edge has been certified to run on the following:
• Windows XP Professional® operating system (32 bit or 64 bit)
• Windows Vista Business® or Vista Enterprise® operating system (32 bit or 64 bit)
• Internet Explorer 7.0 (IE 6.0 minimum)
This Update can be instaled installed on top of Version: 20.00.00.96, 20.00.01.08,
20.00.02.03, or 20.00.03.03.
Note: Updates are all inclusive and can be installed on top of the base release
or any released UPdate.
--------------------
End of Release Notes
--------------------
-------------------
Installation Notes:
-------------------
After downloading the Update to your machine, dbl click the downloaded file
and the Update will install.
-------------------
End of Installation
-------------------
----------------------------------------------------------
This Update addresses the following Customer Reported PRs:
----------------------------------------------------------
=====Assembly=====
PR 1612509: Fixed a problem with line creation in XpresRoute on simplified parts
PR 1620041: Fixed a problem where Frame components are surfaces after Save As
PR 5856651: Fixed a problem where JT file open is slow
PR 5871038: Fixed a problem where Solid Edge crashed when adding parts to an existing assembly pattern
PR 5867700: Fixed a problem where Solid Edge crashed after creating a swept protrusion and saving the assembly.
=====Part=====
PR 1629172: Fixed a problem where Solid Edge is crashing when executing Bluesurf command
PR 5861912: Fixed a problem where SEPartx.ocx does not work in Excel
PR 1623107: Fixed a problem where using flat pattern in V19 flattens the model but "removes" one of the flanges
PR 1633469: Fixed a problem where the Sphere color changes when zooming in.
PR 1618523: Fixed a problem where Solid Edge crashes when include is used in 2 open assemblies.
=====Draft=====
PR 5862532: Fixed a problem where a DWG file created from Solid Edge is not opening in AutoCAD
PR 5814536: Fixed a problem where a threaded finite hole does not show thread lines in hidden orientation.
=====API=====
PR 5855377: Fixed a problem with GetSaveAsFileName() Enhancement Request where the user can now obtain the default filters used by the command by passing in "default" or "default_XXX" where XXX is par, asm, dft, pwd, psm or familyasm. If the simple "default" is supplied, Edge will get the appropriate filter set for the active document or a part document if no document is active.
=====Insight=====
PR 1634261: Fixed a problem where files are left checked out after editing.
PR 5867701: Fixed a problem where Solid Edge search is not finding all documents when Look in contains multiple paths
---
End
---