Solid Edge ST6 SDK
Solid Edge V20 SP8 - Readme

--------------
Legal Notices
--------------
©2008 Siemens Product Lifecycle Management Software Inc.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.

Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024


--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        20.00.08.04
Date:           23-Jul-2008

This release of Solid Edge has been certified to run on the following:
    • Windows XP Professional® operating system (32 bit or 64 bit)
    • Windows Vista Business® or Vista Enterprise® operating system (32 bit or 64 bit)
    • Internet Explorer 7.0 (IE 6.0 minimum)

This Update can be instaled installed on top of Version: 20.00.00.96, 20.00.01.08,
20.00.02.03, 20.00.03.03, 20.00.04.04, 20.00.05.05, 20.00.06.06, or 20.00.07.04.

Note: Updates are all inclusive and can be installed on top of the base release
      or any released UPdate.

--------------------
End of Release Notes
--------------------

-------------------
Installation Notes:
-------------------

After downloading the Update to your machine, dbl click the downloaded file
and the Update will install.

-------------------
End of Installation
-------------------

----------------------------------------------------------
This Update addresses the following Customer Reported PRs:
----------------------------------------------------------

=====Assembly=====

PR 5847501: Fixed problem that caused an abort when applying an angular relationship
PR 5906839: Fixed a problem where the Assembly Pattern command is creating extra occurrences
PR 1665948: Fixed a problem where parts were not listed in Edgebar and cannot be deleted
PR 2098485: Fixed a problem that caused an abort when opening Physical Property Manager
PR 1625279: Fixed a problem where Interpart-Manager lists the wrong information
PR 2097711: Fixed a problem where the mass of physical properties is not correct
PR 1664488: Fixed a problem where you cannot generate a standard part
PR 5969985: Fixed a problem that caused an abort based on auto-submitted crashlogs
PR 2097514: Fixed a problem where FlashFit surfaces are locating in incorrect order
PR 5971808: Fixed a problem that caused unpredictable arc dimensions in XpresRoute
PR 5972224: Fixed a problem where helical spur gears are being created incorrectly
PR 1623215: Fixed a problem where the "Edit Adjustable Part" command was missing in Solid Edge Foundation.
PR 5728742: Fixed a problem where you cannot create a simplified assembly
PR 5984610: Fixed a problem where Frames cannot be seen in a simplified assembly saved as a part.
PR 2098304: Fixed a problem where editing a tube radii returns to default after Transfer
PR 5964249: Fixed a problem with performance and memory issues editing and updating a weldment.
PR 5784262: Fixed a problem with When placing simplified assy, components disappear after dragging into graphics
PR 1662218: Fixed a problem with a Standard parts error, unsupported format of a non-CAD document
PR 1668572: Fixed a problem where you are unable to change frame end conditions to butt2
PR 2090384: Fixed a problem where Save As RTF format garbles Japanese text
PR 5988608: Fixed problems with assembly feature performance.

=====Part=====

PR 2102153: Fixed a problem that caused an abort when setting the maximum density is 0.5
PR 5825612: Fixed a problem where UG assembly file does not translate correctly in Solid Edge V20.
PR 1662715: Fixed a problem that caused an abort after update all.
PR 2101442: Fixed a problem where you cannot create Contour Flange when setting Bend radius=0mm
PR 1672651: Fixed a problem where you are unable to flatten a sheet metal part with a chamfer
PR 1661859: Fixed a problem where Model view takes a very long time in View and Markup.
PR 5785898: Fixed a problem where Solid Edge aborts opening a Parasolid file.
PR 1668264: Fixed a problem with open JT file causing duplicate the file names.

=====Draft=====

PR 1639511: Fixed a problem where dimensions are not correct when opening a DXF file.
PR 2098559: Fixed a problem where dimensions are missing in imported dxf
PR 5957864: Fixed a problem that caused an abort during create/update of a view with a PMI model view.
PR 5786340: Fixed a problem where the Elements on the Auto Hide layer are being exported as visible
PR 2101520: Fixed a problem where views with old tubes failed to place correctly.
PR 2103451: Fixed a problem where a "Surface Texture Symbol" cannot be exported to DXF.
PR 2101453: Fixed a problem where dimension and lines overlap when exported to DXF
PR 5802490: Fixed a problem where AutoCAD Ft-In dimensions do not translate properly
PR 5991964: Fixed a problem with "Error: no reference" displayed in callouts linked to missing properties

=====Insight=====
 
PR 1662107: Fixed a problem where create in place does not warn user in certain scenarios
PR 5941878: Fixed a problem where a new part is left in a checked out state when draft is checked in and closed
PR 1637467: Fixed a problem where Version comments (Edit Profile) are not listed in version history in SharePoint
PR 5957759: Fixed a problem where older files from cache overwrite newer files on Insight/SharePoint server

=====API=====
 
PR 5979480: Fixed a problem where DraftDataAPI.dll had a dependency on SEAlloc.dll
PR 1615362: Fixed a problem with API-open/close-events causing corrupt pointers
PR 5959193: Fixed a problem with the compatibility of SEPartReader.DLL on Vista


---
End
---