Solid Edge ST6 SDK
Solid Edge V20 SP9 - Readme

--------------
Legal Notices
--------------
©2008 Siemens Product Lifecycle Management Software Inc.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.

Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024


--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        20.00.09.03
Date:           27-Aug-2008


This release of Solid Edge has been certified to run on the following:
    • Windows XP Professional® operating system (32 bit or 64 bit)
    • Windows Vista Business® or Vista Enterprise® operating system (32 bit or 64 bit)
    • Internet Explorer 7.0 (IE 6.0 minimum)

This Update can be instaled installed on top of Version: 20.00.00.96, 20.00.01.08,
20.00.02.03, 20.00.03.03, 20.00.04.04, 20.00.05.05, 20.00.06.06, 20.00.07.04, or
20.00.08.04.

Note: Updates are all inclusive and can be installed on top of the base release
      or any released UPdate.

--------------------
End of Release Notes
--------------------

-------------------
Installation Notes:
-------------------

After downloading the Update to your machine, dbl click the downloaded file
and the Update will install.

-------------------
End of Installation
-------------------

----------------------------------------------------------
This Update addresses the following Customer Reported PRs:
----------------------------------------------------------

=====Assembly=====

PR 1676717: Fixed a problem where Rack and Pinion Gears produce the wrong results.
PR 1641424: Fixed a problem where Solid Edge was crashing when working with zones.
PR 6006563: Fixed a problem where a specific Assembly file aborts on save.
PR 2105941: Fixed a problem where the "Explode" command caused Solid Edge to crash.
PR 5874510: Fixed a problem where Solid Edge entered into a Not Responding state while simplifying an assembly.
PR 5899813: Fixed a problem where Solid Edge was aborting  when editing a weld label.
PR 5872719: Fixed a problem where editing a Stitch Weld assembly feature causes an abort.
PR 1672958: Fixed a problem saving a simplified assembly in a folder where there is an existing file with the same name.
PR 2082240: Fixed a problem where "Export Display Only" is not working when edit into sub-assembly
PR 5842365: Fixed a problem where saved configurations are lost converting an assembly into an FOA.
PR 1674763: Fixed a problem where match coordinate system doesn’t locate the CS when assembly features exist
PR 1599941: Fixed a problem where threaded holes in assembly have incorrect diameters.
PR 2104933: Fixed a problem where you can not include normal to face using fence select
PR 5950256: Fixed a problem where Solid Edge aborts when saving family of assembly file.
PR 5943101: Fixed a problem where Solid Edge crashes when opening JT file created by IDEAS
PR 5902637: Fixed a problem where Solid Edge crashes when opening a part from draft and in assembly.
PR 5782973: Fixed a problem where IDEAS data Migration fails to migrate drawing, and locks up the process

=====Part=====

PR 5921066: Fixed a problem where Hole callouts for patterned counterbore and countersink holes are wrong
PR 2100883: Fixed a problem where a round disappears when part is recomputed
PR 5844833: Fixed a problem where a Sheet metal part is displaying the wrong angle in draft.
PR 6000242: Fixed a problem where you are unable to import an STL file.

=====Draft=====

PR 1656622: Fixed a problem where an Image is disappearing after pasting.
PR 1585174: Fixed a problem where connecters in a Block are not correct. 
PR 5982657: Fixed a problem where a Microstation 2-D dgn file causes Solid Edge to crash
PR 2103557: Fixed a problem where Blocks are not exporting to dxf on Japanese XP.
PR 1670678: Fixed a problem where Solid Edge Line width to ACAD Color Mapping is not working for dimensions
PR 6000905: Fixed a problem where opening DGN file causes Solid Edge to abort
PR 5971763: Fixed a problem where you are unable to Copy/Move multiple elements in Draw in View. 
PR 1619152: Fixed a problem where a drawing border is not saved out in pdf
PR 5841236: Fixed a problem where zooming with Ctrl+RMB is deselecting geometry
PR 1616825: Fixed a problem where hitting 5 on Numeric Pad selects Endpoint
PR 5994535: Fixed a problem where drawing views are not exported using "Translate drawing views as blocks"
PR 2104940: Fixed a problem where hidden layers were not hidden after drawing view converted to 2D.

=====Insight/=====
 
PR 1675808: Fixed a problem where search For Broken Links crashes on Hebrew OS.
PR 5991256: Fixed a problem where you are unable to change Doc No and Rev No in Rev Mgr for certain parts.
PR 5549874: Fixed a problem where parts are shown as Designed even though use Simplified parts option is used.
PR 5706206: Fixed a problem where Insight warnings appear for each file when saving assy.


---
End
---