| Programmer's Guide > Solid Edge > Environments > Part and Sheet Metal > Working with Dimensions |
Solid Edge allows you to place and edit dimensions on elements. In the Profile environment, dimension objects control the size and orientation of geometry.
Dimensions can be linear, radial, or angular. Dimensions supply information about the measurements of elements, such as the angle of a line or the distance between two points. A dimension is related to the element on which it is placed. In the Profile environment, the dimensions control the geometry; if the dimension changes, the geometry updates.
In a Part document, the Dimensions collection is accessed through the Profile object. The Dimensions collection provides the methods for placing dimensions and for iterating through all the dimensions on the entire sheet or profile.
Linear Dimensions
A linear dimension measures the distance between two or more elements, the length of a line, or an arc's length. For a complete description of the properties that define how a linear dimension is placed, see the Programming with Solid Edge on-line Help.
Radial Dimensions
Radial dimensions measure the radius or diameter at a point on the element. These dimensions are similar except that they show the radius or diameter value depending on the type. With the ProjectionArc and TrackAngle properties, you can define the measurement point on the element.
Angular Dimensions
Angular dimensions measure the angle between two lines or three points. An angular dimension defines two intersecting vectors and four minor sectors. These sectors are distinguished according to whether the angle is measured in the sector where the vector direction goes outward from the intersection point or comes inward, and whether the angle is measured in the clockwise or counterclockwise direction.
The angles are always measured in the counterclockwise direction with both vector directions going outward from the intersection point (sector one condition). To measure in any other angle, certain properties are set so that the dimension object modifies the vector direction and computes the angle.
In the Profile environment, driving dimensions control the elements to which they refer. When you edit a driving dimension, the geometry of the element that is related to that dimension is modified.
You can place dimensions only on existing elements. A set of Add methods is provided on the Dimensions collection, one for each type of dimension. The element to which the dimension is attached determines the type of dimension (driving or driven) that will be placed. The Add methods on the Dimensions collection object take minimal input and place the dimensions with specific default values.
When you place dimensions between two elements interactively, the dimensions are measured at a specific location on an element. For example, when you place a dimension between the end points of two lines, you select one end of each line. When you place dimensions through automation, you specify a point on the element and a key point flag to define the dimension.
In the following program, four lines are drawn and connected with key point relationships. The lengths of two of the lines and the distance between two lines are dimensioned. The dimension is set to be a driving dimension so it will control the length and position of the geometry. The sample also shows how to modify a dimension style by changing the units of measurement of one of the dimensions to meters.
![]() |
See Handling 'Application is Busy' and 'Call was Rejected By Callee' errors for information regarding the use of OleMessageFilter. |
| Placing Dimensions in Visual Basic .NET |
Copy Code
|
|---|---|
Imports SolidEdgeConstants Imports System.Runtime.InteropServices Module Program <STAThread()> _ Sub Main() Dim objApplication As SolidEdgeFramework.Application = Nothing Dim objDocuments As SolidEdgeFramework.Documents = Nothing Dim objPart As SolidEdgePart.PartDocument = Nothing Dim objProfileSets As SolidEdgePart.ProfileSets = Nothing Dim objProfileSet As SolidEdgePart.ProfileSet = Nothing Dim objProfiles As SolidEdgePart.Profiles = Nothing Dim objProfile As SolidEdgePart.Profile = Nothing Dim objRefPlanes As SolidEdgePart.RefPlanes = Nothing Dim objRefPlane As SolidEdgePart.RefPlane = Nothing Dim objLines2d As SolidEdgeFrameworkSupport.Lines2d = Nothing Dim aLine2d(0 To 3) As SolidEdgeFrameworkSupport.Line2d Dim objRelations2d As SolidEdgeFrameworkSupport.Relations2d = Nothing Dim objDimensions As SolidEdgeFrameworkSupport.Dimensions = Nothing Dim objDimension As SolidEdgeFrameworkSupport.Dimension = Nothing Dim objDimStyle As SolidEdgeFrameworkSupport.DimStyle = Nothing Dim i As Integer Try OleMessageFilter.Register() ' Connect to a running instance of Solid Edge objApplication = Marshal.GetActiveObject("SolidEdge.Application") ' Get a reference to the documents collection objDocuments = objApplication.Documents ' Add a Part document objPart = objDocuments.Add("SolidEdge.PartDocument") ' Get a reference to the ref planes collection objRefPlanes = objPart.RefPlanes ' Get a reference to the first reference plane objRefPlane = objRefPlanes.Item(1) ' Get a reference to the profile sets collection objProfileSets = objPart.ProfileSets ' Add a new profile set objProfileSet = objProfileSets.Add() ' Get a reference to the profiles collection objProfiles = objProfileSet.Profiles ' Add a new profile on the selected reference plane objProfile = objProfiles.Add(objRefPlane) ' Get a reference to the lines 2d collection objLines2d = objProfile.Lines2d ' Get a reference to the relations 2d collection objRelations2d = objProfile.Relations2d ' Get a reference to the dimensions collection objDimensions = objProfile.Dimensions ' Draw the geometry. aLine2d(0) = objLines2d.AddBy2Points(0, 0, 0.1, 0) aLine2d(1) = objLines2d.AddBy2Points(0.1, 0, 0.1, 0.1) aLine2d(2) = objLines2d.AddBy2Points(0.1, 0.1, 0, 0.05) aLine2d(3) = objLines2d.AddBy2Points(0, 0.05, 0, 0) ' Add endpoint relationships between the lines objRelations2d.AddKeypoint( _ aLine2d(0), _ KeypointIndexConstants.igLineEnd, _ aLine2d(1), _ KeypointIndexConstants.igLineStart) objRelations2d.AddKeypoint( _ aLine2d(1), _ KeypointIndexConstants.igLineEnd, _ aLine2d(2), _ KeypointIndexConstants.igLineStart) objRelations2d.AddKeypoint( _ aLine2d(2), _ KeypointIndexConstants.igLineEnd, _ aLine2d(3), _ KeypointIndexConstants.igLineStart) objRelations2d.AddKeypoint( _ aLine2d(3), _ KeypointIndexConstants.igLineEnd, _ aLine2d(0), _ KeypointIndexConstants.igLineStart) ' Add dimensions, and change the dimension units to meters objDimension = objDimensions.AddLength(aLine2d(1)) objDimension.Constraint = True objDimStyle = objDimension.Style objDimStyle.PrimaryUnits = _ DimLinearUnitConstants.igDimStyleLinearMeters objDimension = objDimensions.AddLength(aLine2d(3)) objDimension.Constraint = True objDimStyle = objDimension.Style objDimStyle.PrimaryUnits = _ DimLinearUnitConstants.igDimStyleLinearMeters objDimension = objDimensions.AddDistanceBetweenObjects( _ aLine2d(1), 0.1, 0.1, 0, False, _ aLine2d(2), 0, 0.05, 0, False) objDimension.Constraint = True objDimStyle = objDimension.Style objDimStyle.PrimaryUnits = _ DimLinearUnitConstants.igDimStyleLinearMeters Catch ex As Exception Console.WriteLine(ex.Message) Finally OleMessageFilter.Revoke() End Try End Sub End Module |
|
| Placing Dimensions in C# |
Copy Code
|
|---|---|
using SolidEdgeConstants; using System; using System.Reflection; using System.Runtime.InteropServices; namespace SolidEdge.SDK { class Program { [STAThread] static void Main(string[] args) { SolidEdgeFramework.Application application = null; SolidEdgeFramework.Documents documents = null; SolidEdgePart.PartDocument part = null; SolidEdgePart.ProfileSets profileSets = null; SolidEdgePart.ProfileSet profileSet = null; SolidEdgePart.Profiles profiles = null; SolidEdgePart.Profile profile = null; SolidEdgePart.RefPlanes refPlanes = null; SolidEdgePart.RefPlane refPlane = null; SolidEdgeFrameworkSupport.Lines2d lines2d = null; SolidEdgeFrameworkSupport.Line2d[] aLine2d = new SolidEdgeFrameworkSupport.Line2d[4]; SolidEdgeFrameworkSupport.Relations2d relations2d = null; SolidEdgeFrameworkSupport.Dimensions dimensions = null; SolidEdgeFrameworkSupport.Dimension dimension = null; SolidEdgeFrameworkSupport.DimStyle dimStyle = null; try { OleMessageFilter.Register(); // Connect to a running instance of Solid Edge application = (SolidEdgeFramework.Application) Marshal.GetActiveObject("SolidEdge.Application"); // Get a reference to the documents collection documents = application.Documents; // Add a Part document part = (SolidEdgePart.PartDocument) documents.Add("SolidEdge.PartDocument", Missing.Value); // Get a reference to the ref planes collection refPlanes = part.RefPlanes; // Get a reference to the first reference plane refPlane = refPlanes.Item(1); // Get a reference to the profile sets collection profileSets = part.ProfileSets; // Add a new profile set profileSet = profileSets.Add(); // Get a reference to the profiles collection profiles = profileSet.Profiles; // Add a new profile on the selected reference plane profile = profiles.Add(refPlane); // Get a reference to the lines 2d collection lines2d = profile.Lines2d; // Get a reference to the relations 2d collection relations2d = (SolidEdgeFrameworkSupport.Relations2d) profile.Relations2d; // Get a reference to the dimensions collection dimensions = (SolidEdgeFrameworkSupport.Dimensions) profile.Dimensions; // Draw the geometry. aLine2d[0] = lines2d.AddBy2Points(0, 0, 0.1, 0); aLine2d[1] = lines2d.AddBy2Points(0.1, 0, 0.1, 0.1); aLine2d[2] = lines2d.AddBy2Points(0.1, 0.1, 0, 0.05); aLine2d[3] = lines2d.AddBy2Points(0, 0.05, 0, 0); // Add endpoint relationships between the lines relations2d.AddKeypoint( aLine2d[0], (int)KeypointIndexConstants.igLineEnd, aLine2d[1], (int)KeypointIndexConstants.igLineStart, Missing.Value); relations2d.AddKeypoint( aLine2d[1], (int)KeypointIndexConstants.igLineEnd, aLine2d[2], (int)KeypointIndexConstants.igLineStart, Missing.Value); relations2d.AddKeypoint( aLine2d[2], (int)KeypointIndexConstants.igLineEnd, aLine2d[3], (int)KeypointIndexConstants.igLineStart, Missing.Value); relations2d.AddKeypoint( aLine2d[3], (int)KeypointIndexConstants.igLineEnd, aLine2d[0], (int)KeypointIndexConstants.igLineStart, Missing.Value); // Add dimensions, and change the dimension units to meters dimension = dimensions.AddLength(aLine2d[1]); dimension.Constraint = true; dimStyle = dimension.Style; dimStyle.PrimaryUnits = SolidEdgeFrameworkSupport.DimLinearUnitConstants.igDimStyleLinearMeters; dimension = dimensions.AddLength(aLine2d[3]); dimension.Constraint = true; dimStyle = dimension.Style; dimStyle.PrimaryUnits = SolidEdgeFrameworkSupport.DimLinearUnitConstants.igDimStyleLinearMeters; dimension = dimensions.AddDistanceBetweenObjects( aLine2d[1], 0.1, 0.1, 0, false, aLine2d[2], 0, 0.05, 0, false); dimension.Constraint = true; dimStyle = dimension.Style; dimStyle.PrimaryUnits = SolidEdgeFrameworkSupport.DimLinearUnitConstants.igDimStyleLinearMeters; } catch (System.Exception ex) { Console.WriteLine(ex.Message); } finally { OleMessageFilter.Revoke(); } } } } |
|
When working interactively with the Variable Table, both variables and dimensions are displayed in the table. This enables you to create formulas using the values of dimensions and also have formulas that drive the values of dimensions. In this workflow, there is no apparent difference between variables and dimensions. Internally, however, variables and dimensions are two distinct types of objects that have their own unique collections, properties, and methods.
The Variables collection allows you to work with dimensions in the context of variables through several methods on the collection. These methods include Edit, GetFormula, GetName, PutName, Query, and Translate. The following program uses dimensions through the Variables collection. The following programs assume that Solid Edge is running and in the Profile environment.
![]() |
See Handling 'Application is Busy' and 'Call was Rejected By Callee' errors for information regarding the use of OleMessageFilter. |
| Accessing Dimensions through the Variable Table in Visual Basic .NET |
Copy Code
|
|---|---|
Imports System.Runtime.InteropServices Module Program <STAThread()> _ Sub Main() Dim objApplication As SolidEdgeFramework.Application = Nothing Dim objPart As SolidEdgePart.PartDocument = Nothing Dim objProfileSets As SolidEdgePart.ProfileSets = Nothing Dim objProfileSet As SolidEdgePart.ProfileSet = Nothing Dim objProfiles As SolidEdgePart.Profiles = Nothing Dim objProfile As SolidEdgePart.Profile = Nothing Dim objVariables As SolidEdgeFramework.Variables = Nothing Dim objVariable As Object = Nothing Dim objLines2d As SolidEdgeFrameworkSupport.Lines2d = Nothing Dim objLine2d As SolidEdgeFrameworkSupport.Line2d = Nothing Dim objDimensions As SolidEdgeFrameworkSupport.Dimensions = Nothing Dim objDimension1 As SolidEdgeFrameworkSupport.Dimension = Nothing Dim objDimension2 As SolidEdgeFrameworkSupport.Dimension = Nothing Dim objVariableList As SolidEdgeFramework.VariableList = Nothing Dim sName As String Dim sFormula As String Try OleMessageFilter.Register() ' Connect to a running instance of Solid Edge objApplication = Marshal.GetActiveObject("SolidEdge.Application") ' Get a reference to the active document objPart = objApplication.ActiveDocument ' Get a reference to the active document objProfileSets = objPart.ProfileSets ' Get a reference to the profile set objProfileSet = objProfileSets.Item(objProfileSets.Count) ' Get a reference to the profiles collection objProfiles = objProfileSet.Profiles ' Get a reference to the profile objProfile = objProfiles.Item(1) ' Get a reference to the variables collection objVariables = objPart.Variables ' Get a reference to the lines2d collection objLines2d = objProfile.Lines2d ' Get a reference to the dimensions collection objDimensions = objProfile.Dimensions ' Create a new line objLine2d = objLines2d.AddBy2Points(0, 0, 0.1, 0.1) ' Place a dimension on the line to control its length objDimension1 = objDimensions.AddLength(objLine2d) ' Make the dimension a driving dimension objDimension1.Constraint = True ' Create a second line objLine2d = objLines2d.AddBy2Points(0, 0.1, 0.1, 0.2) ' Place a dimension on the line to control its length objDimension2 = objDimensions.AddLength(objLine2d) ' Make the dimension a driving dimension objDimension2.Constraint = True ' Assign a name to the dimension placed on the first line objVariables.PutName(objDimension1, "Dimension1") ' Retrieve the system name of the second dimension, and display ' it in the debug window sName = objVariables.GetName(objDimension2) Console.WriteLine(String.Format("Dimension = {0}", sName)) ' Edit the formula of the second dimension to be half ' the value of the first dimension objVariables.Edit(sName, "Dimension1/2.0") ' Retrieve the formula from the dimension, and print it to the ' debug window to verify sFormula = objVariables.GetFormula(sName) Console.WriteLine(String.Format("Formula = {0}", sFormula)) ' This demonstrates the ability to reference a dimension object ' by its name objDimension1 = objVariables.Translate("Dimension1") ' To verify a dimension object was returned, change its ' TrackDistance property to cause the dimension to change objDimension1.TrackDistance = objDimension1.TrackDistance * 2 ' Use the Query method to list all all user-defined ' variables and user-named Dimension objects and ' display in the debug window objVariableList = objVariables.Query("*") For Each objVariable In objVariableList Console.WriteLine(objVariables.GetName(objVariable)) Next Catch ex As Exception Console.WriteLine(ex.Message) Finally OleMessageFilter.Revoke() End Try End Sub End Module |
|
| Accessing Dimensions through the Variable Table in C# |
Copy Code
|
|---|---|
using SolidEdgeFramework; using System; using System.Runtime.InteropServices; namespace SolidEdge.SDK { class Program { [STAThread] static void Main(string[] args) { SolidEdgeFramework.Application application = null; SolidEdgePart.PartDocument part = null; SolidEdgePart.ProfileSets profileSets = null; SolidEdgePart.ProfileSet profileSet = null; SolidEdgePart.Profiles profiles = null; SolidEdgePart.Profile profile = null; SolidEdgeFramework.Variables variables = null; Object oVariable = null; SolidEdgeFrameworkSupport.Lines2d lines2d = null; SolidEdgeFrameworkSupport.Line2d line2d = null; SolidEdgeFrameworkSupport.Dimensions dimensions = null; SolidEdgeFrameworkSupport.Dimension dimension1 = null; SolidEdgeFrameworkSupport.Dimension dimension2 = null; SolidEdgeFramework.VariableList variableList = null; String sName; String sFormula; try { OleMessageFilter.Register(); // Connect to a running instance of Solid Edge application = (SolidEdgeFramework.Application) Marshal.GetActiveObject("SolidEdge.Application"); // Get a reference to the active document part = (SolidEdgePart.PartDocument) application.ActiveDocument; // Get a reference to the profile sets collection profileSets = part.ProfileSets; // Get a reference to the profile set profileSet = profileSets.Item(profileSets.Count); // Get a reference to the profiles collection profiles = profileSet.Profiles; // Get a reference to the profile profile = profiles.Item(1); // Get a reference to the variables collection variables = (SolidEdgeFramework.Variables)part.Variables; // Get a reference to the lines2d collection lines2d = profile.Lines2d; // Get a reference to the dimensions collection dimensions = (SolidEdgeFrameworkSupport.Dimensions) profile.Dimensions; // Create a line line2d = lines2d.AddBy2Points(0, 0, 0.1, 0.1); // Place a dimension on the line to control its length dimension1 = dimensions.AddLength(line2d); // Make the dimension a driving dimension dimension1.Constraint = true; // Create a second line line2d = lines2d.AddBy2Points(0, 0.1, 0.1, 0.2); // Place a dimension on the line to control its length dimension2 = dimensions.AddLength(line2d); // Make the dimension a driving dimension dimension2.Constraint = true; // Assign a name to the dimension placed on the first line variables.PutName(dimension1, "Dimension1"); // Retrieve the system name of the second dimension, and display // it in the debug window sName = variables.GetName(dimension2); Console.WriteLine(String.Format("Dimension = {0}", sName)); // Edit the formula of the second dimension to be half // the value of the first dimension variables.Edit(sName, "Dimension1/2.0"); // Retrieve the formula from the dimension, and print it to the // debug window to verify sFormula = variables.GetFormula(sName); Console.WriteLine(String.Format("Formula = {0}", sFormula)); // This demonstrates the ability to reference a dimension object // by its name dimension1 = (SolidEdgeFrameworkSupport.Dimension) variables.Translate("Dimension1"); // To verify a dimension object was returned, change its // TrackDistance property to cause the dimension to change dimension1.TrackDistance = dimension1.TrackDistance * 2; // Use the Query method to list all all user-defined // variables and user-named Dimension objects and // display in the debug window variableList = (SolidEdgeFramework.VariableList) variables.Query("*", null, null, false); for (int i = 1; i <= variableList.Count; i++) { oVariable = variableList.Item(i); Console.WriteLine(variables.GetName(oVariable)); } } catch (System.Exception ex) { Console.WriteLine(ex.Message); } finally { OleMessageFilter.Revoke(); } } } } |
|