Solid Edge ST6 SDK
Working with Reference Planes

A reference axis defines the axis of revolution for a revolved feature. Reference axes are usually created in the Profile environment when a user defines the profile of the revolution. Two objects—the collection object, RefAxes, and the instance object, RefAxis—are available to enable you to manipulate reference axes in your models.

The following programs connect to a running instance of Solid Edge, creates an Assembly document and places an assembly reference plane using the AddAngularByAngle method. Then the program creates a Part document and places a reference plane using the AddParallelByDistance method.

See Handling 'Application is Busy' and 'Call was Rejected By Callee' errors for information regarding the use of OleMessageFilter.
Creating Reference Planes in Visual Basic .NET
Copy Code
Imports SolidEdgePart
Imports System.Runtime.InteropServices

Module Program
    <STAThread()> _
    Sub Main()
        Dim objApplication As SolidEdgeFramework.Application = Nothing
        Dim objDocuments As SolidEdgeFramework.Documents = Nothing
        Dim objAssembly As SolidEdgeAssembly.AssemblyDocument = Nothing
        Dim objAsmRefPlanes As SolidEdgeAssembly.AsmRefPlanes = Nothing
        Dim objAsmRefPlane As SolidEdgeAssembly.AsmRefPlane = Nothing
        Dim objPPlane As SolidEdgeAssembly.AsmRefPlane = Nothing
        Dim objPart As SolidEdgePart.PartDocument = Nothing
        Dim objRefPlanes As SolidEdgePart.RefPlanes = Nothing
        Dim objRefPlane As SolidEdgePart.RefPlane = Nothing

        Try
            OleMessageFilter.Register()

            ' Connect to a running instance of Solid Edge
            objApplication = Marshal.GetActiveObject("SolidEdge.Application")

            ' Access the Documents collection object
            objDocuments = objApplication.Documents

            ' Add an Assembly document
            objAssembly = objDocuments.Add("SolidEdge.AssemblyDocument")

            ' Access the AsmRefPlanes collection object
            objAsmRefPlanes = objAssembly.AsmRefPlanes

            ' Create a reference plane at an angle to a
            ' principal reference plane
            objPPlane = objAsmRefPlanes.Item(2)

            ' Add a new reference plane
            objAsmRefPlane = objAsmRefPlanes.AddAngularByAngle( _
              objPPlane, _
                          (2 * Math.PI / 3), _
              objAsmRefPlanes.Item(1), _
              ReferenceElementConstants.igPivotEnd, _
              ReferenceElementConstants.igNormalSide, _
              True)

            ' Add a Part document
            objPart = objDocuments.Add("SolidEdge.PartDocument")

            ' Access the RefPlanes collection object
            objRefPlanes = objPart.RefPlanes

            ' Create a global reference plane parallel to the top reference plane
            objRefPlane = objRefPlanes.AddParallelByDistance( _
              objRefPlanes.Item(1), _
              0.1, _
              ReferenceElementConstants.igNormalSide, _
              False)

        Catch ex As Exception
            Console.WriteLine(ex.Message)
        Finally
            OleMessageFilter.Revoke()
        End Try
    End Sub
End Module
Creating Reference Planes in C#
Copy Code
using SolidEdgeFramework;
using SolidEdgePart;
using System;
using System.Reflection;
using System.Runtime.InteropServices;

namespace SolidEdge.SDK
{
    class Program
    {
        [STAThread]
        static void Main(string[] args)
        {
            SolidEdgeFramework.Application application = null;
            SolidEdgeFramework.Documents documents = null;
            SolidEdgeAssembly.AssemblyDocument assembly = null;
            SolidEdgeAssembly.AsmRefPlanes asmRefPlanes = null;
            SolidEdgeAssembly.AsmRefPlane asmRefPlane = null;
            SolidEdgeAssembly.AsmRefPlane pPlane = null;
            SolidEdgePart.PartDocument part = null;
            SolidEdgePart.RefPlanes refPlanes = null;
            SolidEdgePart.RefPlane refPlane = null;

            try
            {
                OleMessageFilter.Register();

                // Connect to a running instance of Solid Edge
                application = (SolidEdgeFramework.Application)
                  Marshal.GetActiveObject("SolidEdge.Application");

                // Access the Documents collection object
                documents = application.Documents;

                // Add an Assembly document
                assembly = (SolidEdgeAssembly.AssemblyDocument)
                  documents.Add("SolidEdge.AssemblyDocument", Missing.Value);

                // Access the AsmRefPlanes collection object
                asmRefPlanes = assembly.AsmRefPlanes;

                // Create a reference plane at an angle to a principal
                // reference plane
                pPlane = asmRefPlanes.Item(2);

                // Add a new reference plane.Add a new reference plane
                asmRefPlane = asmRefPlanes.AddAngularByAngle(
                  pPlane,
                  (2 * Math.PI / 3),
                  asmRefPlanes.Item(1),
                  ReferenceElementConstants.igPivotEnd,
                  ReferenceElementConstants.igNormalSide,
                  true);

                // Add a Part document
                part = (SolidEdgePart.PartDocument)
                  documents.Add("SolidEdge.PartDocument", Missing.Value);

                // Access the RefPlanes collection object
                refPlanes = part.RefPlanes;

                // Create a global reference plane parallel to the top
                // reference plane
                refPlane = refPlanes.AddParallelByDistance(
                  refPlanes.Item(1),
                  0.1,
                  ReferenceElementConstants.igNormalSide,
                  false,
                  Missing.Value,
                  Missing.Value,
                  Missing.Value);

            }
            catch (System.Exception ex)
            {
                Console.WriteLine(ex.Message);
            }
            finally
            {
                OleMessageFilter.Revoke();
            }
        }
    }
}