All Solid Edge document objects implement the SolidEdgeFramework.SolidEdgeDocument interface. This generic interface allows document ambiguity when you don't know what type of document that you're working with.
The following table lists the classes (also called ProgIDs) associated with Solid Edge and each type of document environment. These class names can be used in the Visual Basic function CreateObject and can also be used in the Add method of the Documents object.
| Creating Documents from Visual Basic .NET |
Copy Code
|
Imports System.IO
Imports System.Runtime.InteropServices
Module Program
<DllImport("ole32.dll", CharSet:=CharSet.Unicode, PreserveSig:=False)> _
Function ProgIDFromCLSID(ByRef clsid As Guid) As String
End Function
<STAThread()> _
Sub Main()
Dim objApplication As SolidEdgeFramework.Application = Nothing
Dim objAssemblyDocument As SolidEdgeAssembly.AssemblyDocument = Nothing
Dim objDraftDocument As SolidEdgeDraft.DraftDocument = Nothing
Dim objPartDocument As SolidEdgePart.PartDocument = Nothing
Dim objSheetMetalDocument As SolidEdgePart.SheetMetalDocument = Nothing
Try
OleMessageFilter.Register()
' Connect to Solid Edge
objApplication = Marshal.GetActiveObject("SolidEdge.Application")
' Create new SolidEdgeAssembly.AssemblyDocument.
objAssemblyDocument = CreateSolidEdgeDocument(objApplication, GetType(SolidEdgeAssembly.AssemblyDocument))
' Create new SolidEdgeDraft.DraftDocument.
objDraftDocument = CreateSolidEdgeDocument(objApplication, GetType(SolidEdgeDraft.DraftDocument))
' Create new SolidEdgePart.PartDocument.
objPartDocument = CreateSolidEdgeDocument(objApplication, GetType(SolidEdgePart.PartDocument))
' Create new SolidEdgePart.SheetMetalDocument.
objSheetMetalDocument = CreateSolidEdgeDocument(objApplication, GetType(SolidEdgePart.SheetMetalDocument))
Catch ex As Exception
Console.WriteLine(ex.Message)
Finally
OleMessageFilter.Revoke()
End Try
End Sub
Function CreateSolidEdgeDocument(objApplication As SolidEdgeFramework.Application, objType As Type) As Object
Dim objGuid As Guid
Dim strProgId As String
Dim objDocuments As SolidEdgeFramework.Documents
' Get the Type GUID.
objGuid = objType.GUID
' Get the ProgId for the specified Type.
strProgId = ProgIDFromCLSID(objGuid)
' Get a reference to the Documents object.
objDocuments = objApplication.Documents
' Add specified document.
Return objDocuments.Add(strProgId)
End Function
End Module |
| Creating Documents from C# |
Copy Code
|
using System;
using System.Reflection;
using System.Runtime.InteropServices;
namespace SolidEdge.SDK
{
class Program
{
[DllImport("ole32.dll", CharSet = CharSet.Unicode, PreserveSig = false)]
static extern string ProgIDFromCLSID([In()]ref Guid clsid);
[STAThread]
static void Main(string[] args)
{
SolidEdgeFramework.Application application = null;
SolidEdgeAssembly.AssemblyDocument assemblyDocument = null;
SolidEdgeDraft.DraftDocument draftDocument = null;
SolidEdgePart.PartDocument partDocument = null;
SolidEdgePart.SheetMetalDocument sheetMetalDocument = null;
try
{
OleMessageFilter.Register();
// Connect to a running instance of Solid Edge.
application = (SolidEdgeFramework.Application)
Marshal.GetActiveObject("SolidEdge.Application");
// Create new SolidEdgeAssembly.AssemblyDocument.
assemblyDocument = (SolidEdgeAssembly.AssemblyDocument)
CreateSolidEdgeDocument(application, typeof(SolidEdgeAssembly.AssemblyDocument));
// Create new SolidEdgeDraft.DraftDocument.
draftDocument = (SolidEdgeDraft.DraftDocument)
CreateSolidEdgeDocument(application, typeof(SolidEdgeDraft.DraftDocument));
// Create new SolidEdgePart.PartDocument.
partDocument = (SolidEdgePart.PartDocument)
CreateSolidEdgeDocument(application, typeof(SolidEdgePart.PartDocument));
// Create new SolidEdgePart.SheetMetalDocument.
sheetMetalDocument = (SolidEdgePart.SheetMetalDocument)
CreateSolidEdgeDocument(application, typeof(SolidEdgePart.SheetMetalDocument));
}
catch (System.Exception ex)
{
Console.WriteLine(ex.Message);
}
finally
{
OleMessageFilter.Revoke();
}
}
static object CreateSolidEdgeDocument(SolidEdgeFramework.Application application, Type t)
{
// Get the Type GUID.
Guid guid = t.GUID;
// Get the ProgId for the specified Type.
string progId = ProgIDFromCLSID(ref guid);
// Get a reference to the Documents object.
SolidEdgeFramework.Documents documents = application.Documents;
// Add specified document.
return documents.Add(progId, Missing.Value);
}
}
} |
See Also