| Programmer's Guide > Solid Edge > Frequently Used Programs |
Following function will return Solid Edge Version.
| Get Solid Edge Version |
Copy Code
|
|---|---|
Public Function oGetSolidEdgeVersion() As String Try Dim install As New SEInstallDataLib.SEInstallData Dim strSEVersion As String = String.Empty strSEVersion = install.GetVersion.ToString oReleaseObject(install) oForceGarbageCollection() Return strSEVersion Catch ex As Exception Return Nothing End Try End Function |
|
Following function will return Solid Edge Status.
| Get Solid Edge Version |
Copy Code
|
|---|---|
Public Function oGetSEStatus(ByVal strFName As String) As SolidEdgeFramework.DocumentStatus Dim objPropertySets As SolidEdgeFileProperties.PropertySets = Nothing Try objPropertySets = New SolidEdgeFileProperties.PropertySets Call objPropertySets.Open(strFName, True) Return objPropertySets.Item("ExtendedSummaryInformation").item("Status").value objPropertySets.Close() oReleaseObject(objPropertySets) oForceGarbageCollection() Exit Function Catch ex As Exception Return SolidEdgeFramework.DocumentStatus.igStatusUnknown oReleaseObject(objPropertySets) oForceGarbageCollection() Exit Function End Try End Function |
|
Following function will return Solid Edge Path.
| Get Solid Edge Path |
Copy Code
|
|---|---|
Public Function () As String Dim strSEPath As String = String.Empty Dim install As SEInstallDataLib.SEInstallData = Nothing Try install = New SEInstallDataLib.SEInstallData strSEPath = install.GetInstalledPath Catch ex As Exception Return Nothing Finally oReleaseObject(install) oForceGarbageCollection() End Try Return strSEPath End Function |
|
Following function will Release Solid Edge Object.
| Release Solid Edge Object |
Copy Code
|
|---|---|
Sub (ByVal obj As Object) Try If Not (obj Is Nothing) Then 'this should only be used when programming applications that run in their own process space Marshal.FinalReleaseComObject(obj) End If Catch ex As Exception obj = Nothing End Try End Sub |
|
Following function will kill Solid Edge process.
| Kill Solid Edge |
Copy Code
|
|---|---|
Public Function (ByVal Name As String) As Long Dim LocalProcs As Process() Dim Proc As Process Dim i As Integer LocalProcs = System.Diagnostics.Process.GetProcesses For Each Proc In LocalProcs If UCase(Proc.ProcessName) = UCase(Name) Then Try Proc.Kill() oReleaseObject(Proc) oReleaseObject(LocalProcs) oForceGarbageCollection() Return 0 Catch ex As System.Exception oReleaseObject(Proc) oReleaseObject(LocalProcs) oForceGarbageCollection() Return 1 Exit Function End Try End If i += 1 Next oReleaseObject(Proc) oReleaseObject(LocalProcs) oForceGarbageCollection() Return 1 End Function |
|
Following function will check file attributes.
| Cehck File Attribute |
Copy Code
|
|---|---|
Public Function (ByVal filename As String, ByVal attribute As IO.FileAttributes) As Boolean If IO.File.Exists(filename) Then If (IO.File.GetAttributes(filename) And attribute) > 0 Then Return True Else Return False End If Else Return False End If End Function |
|
Following function will help you to connect to Revision Manager.
| Connecting to Revision Manager |
Copy Code
|
|---|---|
Public Function (ByVal blnAppVisibility As Boolean, ByVal blnDisplayAlerts As Boolean) As Boolean 'to connect to a running instance of Revision Manager Try '("Word.Application") '("Excel.Application") '("RevisionManager.Application") objRevManApp = Marshal.GetActiveObject("RevisionManager.Application") objRevManApp.DisplayAlerts = blnDisplayAlerts objRevManApp.Visible = blnAppVisibility Return True Catch ex As System.Exception 'SE not running then start it Try objRevManApp = Activator.CreateInstance(objRevManType) objRevManApp.DisplayAlerts = blnDisplayAlerts objRevManApp.Visible = blnAppVisibility Return True Catch ex1 As Exception Return False End Try End Try Return False End Function |
|
Following function will determine whether File Name is valid or not.
| Is Valid File Name? |
Copy Code
|
|---|---|
Public Function (ByVal fn As String) As Boolean Try If System.IO.File.Exists(fn) Then Return True Else Return False End If Catch ex As Exception Return False End Try End Function |
|
Following function will determine if File belongs to Solid Edge or not.
| Is Solid Edge File? |
Copy Code
|
|---|---|
'pass in the full path including filename or just the filename Public Function (ByVal Filename As String) As Boolean Try Dim validFileTypes As String() = {"par", "psm", "asm", "dft", "pwd"} Dim strFileNameOnly As String = String.Empty strFileNameOnly = System.IO.Path.GetFileName(Filename) If strFileNameOnly = String.Empty Then Return False End If If System.IO.Path.HasExtension(strFileNameOnly) Then 'it has an extension now check to see if it is a valid SE one Dim strExtension As String = System.IO.Path.GetExtension(strFileNameOnly) For i As Integer = 0 To validFileTypes.Length - 1 If strExtension.ToLower = "." + validFileTypes(i).ToLower Then Return True End If Next Return False Else Return False End If Catch ex As Exception Return False End Try End Function |
|
Following function will determine if File is Solid Edge Part file or not.
| Is Solid Edge Part File? |
Copy Code
|
|---|---|
'pass in the full path including filename or just the filename Public Function (ByVal Filename As String) As Boolean Dim sExtension As String = Nothing Dim bPart As Boolean = False Try sExtension = System.IO.Path.GetExtension(Filename) If (sExtension.ToLower = ".par") Then Return True Else Return False End If Catch ex As Exception Return False End Try End Function |
|
Following function will determine if File is Solid Edge Sheet Metal file or not.
| Is Solid Edge Sheet Metal File? |
Copy Code
|
|---|---|
'pass in the full path including filename or just the filename Public Function oIsSolidEdgeSheetMetalFile(ByVal Filename As String) As Boolean Dim sExtension As String = Nothing Dim bPart As Boolean = False Try sExtension = System.IO.Path.GetExtension(Filename) If (sExtension.ToLower = ".psm") Then Return True Else Return False End If Catch ex As Exception Return False End Try End Function |
|
Following function will determine if File is Solid Edge Draft file or not.
| Is Solid Edge Draft File? |
Copy Code
|
|---|---|
'pass in the full path including filename or just the filename Public Function (ByVal Filename As String) As Boolean Dim sExtension As String = Nothing Dim bPart As Boolean = False Try sExtension = System.IO.Path.GetExtension(Filename) If (sExtension.ToLower = ".dft") Then Return True Else Return False End If Catch ex As Exception Return False End Try End Function |
|
Following function will determine if File is Solid Edge Assembly file or not.
| Is Solid Edge Assembly File? |
Copy Code
|
|---|---|
'pass in the full path including filename or just the filename Public Function (ByVal Filename As String) As Boolean Dim sExtension As String = Nothing Dim bPart As Boolean = False Try sExtension = System.IO.Path.GetExtension(Filename) If (sExtension.ToLower = ".asm") Then Return True Else Return False End If Catch ex As Exception Return False End Try End Function |
|
Following function will determine if File is Solid Edge Weldment file or not.
| Is Solid Edge Weldment File? |
Copy Code
|
|---|---|
'pass in the full path including filename or just the filename Public Function (ByVal Filename As String) As Boolean Dim sExtension As String = Nothing Dim bPart As Boolean = False Try sExtension = System.IO.Path.GetExtension(Filename) If (sExtension.ToLower = ".pwd") Then Return True Else Return False End If Catch ex As Exception Return False End Try End Function |
|