Solid Edge Revision Manager Object Library > Application Object : SetGlobalParameter Method |
Visual Basic |
---|
Public Function SetGlobalParameter( _ ByVal Parameter As ApplicationGlobalConstants, _ ByVal Value As Variant _ ) As Long |
Value | Description |
---|---|
seApplicationGlobalAdminFileLocation | |
seApplicationGlobalApplyStatusToLinks | |
seApplicationGlobalAvailableRootFolder | |
seApplicationGlobalBaselinedRootFolder | |
seApplicationGlobalCheckInOnClose | |
seApplicationGlobalInReviewRootFolder | |
seApplicationGlobalInsightCacheLocation | |
seApplicationGlobalInsightFolderMappingFileLocation | |
seApplicationGlobalInWorkRootFolder | |
seApplicationGlobalLogFilesLocation | |
seApplicationGlobalLookAheadVersion | |
seApplicationGlobalMakeRevisionsObsolete | |
seApplicationGlobalObsoleteRootFolder | |
seApplicationGlobalOfflineMode | |
seApplicationGlobalReleasedRootFolder | |
seApplicationGlobalRevisionDelimiter | |
seApplicationGlobalSearchScope | |
seApplicationGlobalTeamcenterFormula | |
seApplicationGlobalUpdateDraft | |
seApplicationGlobalUploadOnClose |
Imports RevisionManager Imports System.Runtime.InteropServices Module Example Sub Main() Dim objApplication As RevisionManager.Application = Nothing Dim strLocalCacheLocation As String = "C:\SEInsightCache" Try ' Start Revision Manager. objApplication = New RevisionManager.Application objApplication.SetGlobalParameter(ApplicationGlobalConstants.seApplicationGlobalInsightCacheLocation, strLocalCacheLocation) Catch ex As Exception ' Write any errors to console. Console.WriteLine(ex.Message) Finally ' Release COM Objects. If Not (objApplication Is Nothing) Then objApplication.Quit() Marshal.ReleaseComObject(objApplication) objApplication = Nothing End If End Try End Sub End Module