Solid Edge Revision Manager Object Library
GetLastInsightTransactionMessages Method
Specifies the failed command name.
Specifies the number of documents for which there is error information.
Specifies the documents for which there is error information.
Specifies the error messages for the documents.
Specifies the severity codes for the documents.
Description
This method returns Insight error log information for the last Insight transaction.
Syntax
Visual Basic
Public Function GetLastInsightTransactionMessages( _
   ByRef TransactionString As String, _
   ByRef NumberOfDocuments As Long, _
   ByRef ListofDocumentNamesWithPath As Variant, _
   ByRef ListofMessages As Variant, _
   ByRef ListofSeverityCodes As Variant _
) As Long
Parameters
TransactionString
Specifies the failed command name.
NumberOfDocuments
Specifies the number of documents for which there is error information.
ListofDocumentNamesWithPath
Specifies the documents for which there is error information.
ListofMessages
Specifies the error messages for the documents.
ListofSeverityCodes
Specifies the severity codes for the documents.
Example
Imports RevisionManager
Imports System.Runtime.InteropServices

Module Example

    Sub Main()
        Dim objApplication As RevisionManager.Application = Nothing
        Dim objInsight As RevisionManager.Insight = Nothing
        Dim TransactionString As String = String.Empty
        Dim NumberOfDocuments As Integer
        Dim aListofDocumentNamesWithPath As Object = Nothing
        Dim aListofMessages As Object = Nothing
        Dim aListofSeverityCodes As Object = Nothing

        Try
            ' Start Revision Manager.
            objApplication = New RevisionManager.Application

            ' Get reference to Insight object.
            objInsight = objApplication.Insight

            objInsight.GetLastInsightTransactionMessages(TransactionString, NumberOfDocuments, aListofDocumentNamesWithPath, aListofMessages, aListofSeverityCodes)
        Catch ex As Exception
            ' Write any errors to console.
            Console.WriteLine(ex.Message)
        Finally
            ' Release COM Objects.
            If Not (objInsight Is Nothing) Then
                Marshal.ReleaseComObject(objInsight)
                objInsight = Nothing
            End If

            If Not (objApplication Is Nothing) Then
                objApplication.Quit()
                Marshal.ReleaseComObject(objApplication)
                objApplication = Nothing
            End If
        End Try
    End Sub

End Module
See Also

IInsight Object  | IInsight Members