Solid Edge Revision Manager Object Library
Save Method
Description
Save changes made in all property sets.
Syntax
Visual Basic
Public Function Save() As Long
Example
Imports RevisionManager
Imports System.Runtime.InteropServices

Module Example

    Sub Main()
        Dim objApplication As RevisionManager.Application = Nothing
        Dim objDocument As RevisionManager.Document = Nothing
        Dim objPropertySets As RevisionManager.PropertySets = Nothing

        Try
            ' Start Revision Manager.
            objApplication = New RevisionManager.Application

            objPropertySets = objApplication.PropertySets
            objPropertySets.Open("C:\Part1.par", False)
            objPropertySets.Save()
        Catch ex As Exception
            ' Write any errors to console.
            Console.WriteLine(ex.Message)
        Finally
            ' Release COM Objects.
            If Not (objPropertySets Is Nothing) Then
                Marshal.ReleaseComObject(objPropertySets)
                objPropertySets = Nothing
            End If
            If Not (objDocument Is Nothing) Then
                Marshal.ReleaseComObject(objDocument)
                objDocument = Nothing
            End If
            If Not (objApplication Is Nothing) Then
                objApplication.Quit()
                Marshal.ReleaseComObject(objApplication)
                objApplication = Nothing
            End If
        End Try
    End Sub

End Module
See Also

IPropertySetsAuto Collection  | IPropertySetsAuto Members