Solid Edge Revision Manager Object Library
GetGlobalParameter Method
Specifies the global parameter for which the setting is to be returned.
Returns the setting of the specified global parameter. The data type returned depends on the data being queried. For Application objects, the return data type is Long or Variant. For all other objects, the returned data type is Double.
Syntax
Visual Basic
Public Function GetGlobalParameter( _
   ByVal Parameter As ApplicationGlobalConstants, _
   ByRef Value As Variant _
) As Long
Parameters
Parameter
ValueDescription
seApplicationGlobalAdminFileLocation 
seApplicationGlobalApplyStatusToLinks 
seApplicationGlobalAvailableRootFolder 
seApplicationGlobalBaselinedRootFolder 
seApplicationGlobalCheckInOnClose 
seApplicationGlobalInReviewRootFolder 
seApplicationGlobalInsightCacheLocation 
seApplicationGlobalInsightFolderMappingFileLocation 
seApplicationGlobalInWorkRootFolder 
seApplicationGlobalLogFilesLocation 
seApplicationGlobalLookAheadVersion 
seApplicationGlobalMakeRevisionsObsolete 
seApplicationGlobalObsoleteRootFolder 
seApplicationGlobalOfflineMode 
seApplicationGlobalReleasedRootFolder 
seApplicationGlobalRevisionDelimiter 
seApplicationGlobalSearchScope 
seApplicationGlobalTeamcenterFormula 
seApplicationGlobalUpdateDraft 
seApplicationGlobalUploadOnClose 
Specifies the global parameter for which the setting is to be returned.
Value
Returns the setting of the specified global parameter. The data type returned depends on the data being queried. For Application objects, the return data type is Long or Variant. For all other objects, the returned data type is Double.
Example
Imports RevisionManager
Imports System.Runtime.InteropServices

Module Example

    Sub Main()
        Dim objApplication As RevisionManager.Application = Nothing
        Dim strLocalCacheLocation As String = Nothing

        Try
            ' Start Revision Manager.
            objApplication = New RevisionManager.Application

            objApplication.GetGlobalParameter(ApplicationGlobalConstants.seApplicationGlobalInsightCacheLocation, strLocalCacheLocation)
        Catch ex As Exception
            ' Write any errors to console.
            Console.WriteLine(ex.Message)
        Finally
            ' Release COM Objects.
            If Not (objApplication Is Nothing) Then
                objApplication.Quit()
                Marshal.ReleaseComObject(objApplication)
                objApplication = Nothing
            End If
        End Try
    End Sub

End Module
See Also

IRMgrApp Object  | IRMgrApp Members