Solid Edge Revision Manager Object Library
SetGlobalParameter Method
Specifies the global parameter for which the setting is to be set.
Specifies the setting of the global parameter identified by the Parameter argument.
Description
This method sets the value of a specified global parameter for the referenced Application.
Syntax
Visual Basic
Public Function SetGlobalParameter( _
   ByVal Parameter As ApplicationGlobalConstants, _
   ByVal Value As Variant _
) As Long
Parameters
Parameter
ValueDescription
seApplicationGlobalAdminFileLocation 
seApplicationGlobalApplyStatusToLinks 
seApplicationGlobalAvailableRootFolder 
seApplicationGlobalBaselinedRootFolder 
seApplicationGlobalCheckInOnClose 
seApplicationGlobalInReviewRootFolder 
seApplicationGlobalInsightCacheLocation 
seApplicationGlobalInsightFolderMappingFileLocation 
seApplicationGlobalInWorkRootFolder 
seApplicationGlobalLogFilesLocation 
seApplicationGlobalLookAheadVersion 
seApplicationGlobalMakeRevisionsObsolete 
seApplicationGlobalObsoleteRootFolder 
seApplicationGlobalOfflineMode 
seApplicationGlobalReleasedRootFolder 
seApplicationGlobalRevisionDelimiter 
seApplicationGlobalSearchScope 
seApplicationGlobalTeamcenterFormula 
seApplicationGlobalUpdateDraft 
seApplicationGlobalUploadOnClose 
Specifies the global parameter for which the setting is to be set.
Value
Specifies the setting of the global parameter identified by the Parameter argument.
Example
Imports RevisionManager
Imports System.Runtime.InteropServices

Module Example

    Sub Main()
        Dim objApplication As RevisionManager.Application = Nothing
        Dim strLocalCacheLocation As String = "C:\SEInsightCache"

        Try
            ' Start Revision Manager.
            objApplication = New RevisionManager.Application

            objApplication.SetGlobalParameter(ApplicationGlobalConstants.seApplicationGlobalInsightCacheLocation, strLocalCacheLocation)
        Catch ex As Exception
            ' Write any errors to console.
            Console.WriteLine(ex.Message)
        Finally
            ' Release COM Objects.
            If Not (objApplication Is Nothing) Then
                objApplication.Quit()
                Marshal.ReleaseComObject(objApplication)
                objApplication = Nothing
            End If
        End Try
    End Sub

End Module
See Also

IRMgrApp Object  | IRMgrApp Members