Solid Edge Revision Manager Object Library
CheckOutDocumentsFromServer Method
Specifies the number of documents to check out from the server.
Specifies the documents to check out from the server.
Description
This method checks the documents you specify out from the server.
Syntax
Visual Basic
Public Function CheckOutDocumentsFromServer( _
   ByVal NumberOfDocumentsToCheckOutFromServer As Long, _
   ByVal ListOfDocumentsToCheckOutFromServer As Variant _
) As Long
Parameters
NumberOfDocumentsToCheckOutFromServer
Specifies the number of documents to check out from the server.
ListOfDocumentsToCheckOutFromServer
Specifies the documents to check out from the server.
Example
Imports RevisionManager
Imports System.Runtime.InteropServices

Module Example

    Sub Main()
        Dim objApplication As RevisionManager.Application = Nothing
        Dim objInsight As RevisionManager.Insight = Nothing
        Dim aListOfDocumentsToCheckInToServer(2) As Object

        Try
            ' Start Revision Manager.
            objApplication = New RevisionManager.Application

            ' Get reference to Insight object.
            objInsight = objApplication.Insight

            aListOfDocumentsToCheckInToServer(0) = "D:\InsightCache\Insight\solidvm\Engineering\PreReleased\PreReleasedDocLib\Summit.par"
            aListOfDocumentsToCheckInToServer(1) = "D:\InsightCache\Insight\solidvm\Engineering\PreReleased\PreReleasedDocLib\CDPLayer\CDPlayer.asm"

            objInsight.CheckOutDocumentsFromServer(aListOfDocumentsToCheckInToServer.Length, aListOfDocumentsToCheckInToServer)
        Catch ex As Exception
            ' Write any errors to console.
            Console.WriteLine(ex.Message)
        Finally
            ' Release COM Objects.
            If Not (objInsight Is Nothing) Then
                Marshal.ReleaseComObject(objInsight)
                objInsight = Nothing
            End If

            If Not (objApplication Is Nothing) Then
                objApplication.Quit()
                Marshal.ReleaseComObject(objApplication)
                objApplication = Nothing
            End If
        End Try
    End Sub

End Module
See Also

Insight Object  | Insight Members