Solid Edge Revision Manager Object Library
ExportDocumentsFromServer Method
Specifies the number of documents to export.
Specifies URL paths of the documents to export.
Specifies where to export the specified documents.
Specifies whether to make the specified documents read-only.
Member of the OverWriteFilesOption constant set that specifies whether or not to overwrite documents in the unmanaged export location.
Description
This method exports the specified documents from the server to an unmanaged location you specify.
Syntax
Visual Basic
Public Function ExportDocumentsFromServer( _
   ByVal NumberOfDocumentsToExport As Long, _
   ByVal ListOfDocumentsToExport As Variant, _
   ByVal ExportToLocation As String, _
   ByVal SetDocToReadOnly As Boolean, _
   ByVal OverWriteOption As OverWriteFilesOption _
) As Long
Parameters
NumberOfDocumentsToExport
Specifies the number of documents to export.
ListOfDocumentsToExport
Specifies URL paths of the documents to export.
ExportToLocation
Specifies where to export the specified documents.
SetDocToReadOnly
Specifies whether to make the specified documents read-only.
OverWriteOption
ValueDescription
NoToAll 
YesToAll 
Member of the OverWriteFilesOption constant set that specifies whether or not to overwrite documents in the unmanaged export location.
Example
Imports RevisionManager
Imports System.Runtime.InteropServices

Module Example

    Sub Main()
        Dim objApplication As RevisionManager.Application = Nothing
        Dim objInsight As RevisionManager.Insight = Nothing
        Dim aListOfDocumentsToExport(1) As Object
        Dim ExportToLocation As String
        Dim SetDocToReadOnly As Boolean
        Dim OverWriteOption As Boolean

        Try
            ' Start Revision Manager.
            objApplication = New RevisionManager.Application

            ' Get reference to Insight object.
            objInsight = objApplication.Insight

            aListOfDocumentsToExport(0) = "http://solidvm/Engineering/PreReleased/PreReleasedDocLib/Summit.par"
            aListOfDocumentsToExport(1) = "http://solidvm/Engineering/PreReleased/PreReleasedDocLib/CDPlayer/CDPlayer.asm"
            ExportToLocation = "D:\Temp\ExportFromInsight"
            SetDocToReadOnly = True
            OverWriteOption = RevisionManager.OverWriteFilesOption.NoToAll

            objInsight.ExportDocumentsFromServer(aListOfDocumentsToExport.Length, aListOfDocumentsToExport, ExportToLocation, SetDocToReadOnly, OverWriteOption)
        Catch ex As Exception
            ' Write any errors to console.
            Console.WriteLine(ex.Message)
        Finally
            ' Release COM Objects.
            If Not (objInsight Is Nothing) Then
                Marshal.ReleaseComObject(objInsight)
                objInsight = Nothing
            End If

            If Not (objApplication Is Nothing) Then
                objApplication.Quit()
                Marshal.ReleaseComObject(objApplication)
                objApplication = Nothing
            End If
        End Try
    End Sub

End Module
See Also

Insight Object  | Insight Members