Solid Edge Revision Manager Object Library
MoveDocumentsThroughWorkFlow Method
Specifies the URL path of the file to be assigned a new status.
Member of the DocumentStatus constant set that specifies the new status of the file.
Specifies the number of associated draft files.
Specifies the associated draft files.
Specifies the new status list for the draft files.
Specifies the number of associated revision files.
Specifies the associated revision files.
Specifies the new status list for the revision files.
Description
This method moves the specified file (and optionally its drafts and revisions) to the specified status.
Syntax
Visual Basic
Public Function MoveDocumentsThroughWorkFlow( _
   ByVal FileName As String, _
   ByVal newstatus As DocumentStatus, _
   Optional ByVal NumberOfDraftFiles As Variant, _
   Optional ByVal draftFileList As Variant, _
   Optional ByVal draftFileStatusList As Variant, _
   Optional ByVal NumberOfRevisionFiles As Variant, _
   Optional ByVal revisionFileList As Variant, _
   Optional ByVal RevisionFileStatusList As Variant _
) As Long
Parameters
FileName
Specifies the URL path of the file to be assigned a new status.
newstatus
ValueDescription
igStatusAvailable 
igStatusBaselined 
igStatusInReview 
igStatusInWork 
igStatusObsolete 
igStatusReleased 
Member of the DocumentStatus constant set that specifies the new status of the file.
NumberOfDraftFiles
Specifies the number of associated draft files.
draftFileList
Specifies the associated draft files.
draftFileStatusList
Specifies the new status list for the draft files.
NumberOfRevisionFiles
Specifies the number of associated revision files.
revisionFileList
Specifies the associated revision files.
RevisionFileStatusList
Specifies the new status list for the revision files.
Example
Imports RevisionManager
Imports System.Runtime.InteropServices

Module Example

    Sub Main()
        Dim objApplication As RevisionManager.Application = Nothing
        Dim objInsight As RevisionManager.Insight = Nothing
        Dim DocumentStatus As RevisionManager.DocumentStatus
        Dim strFileName As String
        Dim aDraftFileList(1) As Object
        Dim aDraftFileStatusList(1) As Object
        Dim aRevisionFileList(1) As Object
        Dim aRevisionFileStatusList(1) As Object

        Try
            ' Start Revision Manager.
            objApplication = New RevisionManager.Application

            ' Get reference to Insight object.
            objInsight = objApplication.Insight

            strFileName = "http://solidvm/Engineering/PreReleased/PreReleasedDocLib/CDPlayer/CDPlayer.asm"
            DocumentStatus = DocumentStatus.igStatusAvailable
            aDraftFileList(0) = "http://solidvm/Engineering/PreReleased/PreReleasedDocLib/CDPlayer/test1.dft"
            aDraftFileList(1) = "http://solidvm/Engineering/PreReleased/PreReleasedDocLib/CDPlayer/test2.dft"
            aDraftFileStatusList(0) = DocumentStatus.igStatusInReview
            aDraftFileStatusList(1) = DocumentStatus.igStatusInReview
            aRevisionFileList(0) = "http://solidvm/Engineering/PreReleased/PreReleasedDocLib/CDPlayer/test-1.par"
            aRevisionFileList(1) = "http://solidvm/Engineering/PreReleased/PreReleasedDocLib/CDPlayer/test-2.par"
            aRevisionFileStatusList(0) = DocumentStatus.igStatusBaselined
            aRevisionFileStatusList(1) = DocumentStatus.igStatusBaselined

            objInsight.MoveDocumentsThroughWorkFlow(strFileName, DocumentStatus, aDraftFileList.Length, aDraftFileList, aDraftFileStatusList, aRevisionFileList.Length, aRevisionFileList, aRevisionFileStatusList)
        Catch ex As Exception
            ' Write any errors to console.
            Console.WriteLine(ex.Message)
        Finally
            ' Release COM Objects.
            If Not (objInsight Is Nothing) Then
                Marshal.ReleaseComObject(objInsight)
                objInsight = Nothing
            End If

            If Not (objApplication Is Nothing) Then
                objApplication.Quit()
                Marshal.ReleaseComObject(objApplication)
                objApplication = Nothing
            End If
        End Try
    End Sub

End Module
See Also

Insight Object  | Insight Members