Solid Edge ST7 SDK
Solid Edge ST2 MP10 - Readme

--------------
Legal Notices
--------------
©2010 Siemens Product Lifecycle Management Software Inc.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.

Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024


--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        102.00.10.04
Date:           13-Oct-2010


Maintenance Packs are all inclusive and can be installed on top of the base
release or any released Maintenance Pack.

This Maintenance Pack can be installed on top of Versions:
102.00.00.116, 102.00.01.04, 102.00.02.06, 102.00.03.04. 102.00.04.03, 102.00.05.04,
102.00.06.04, 102.00.07.04,  102.00.08.04, or 102.00.09.05


This release of Solid Edge has been certified to run on the following:

   - Windows XP Professional© operating system (32-bit or 64-bit)
   - Windows Vista Business© or Vista Enterprise© operating system (32-bit or 64-bit)
   - Windows 7 Professional©, Enterprise©, or Ultimate© operating system (32-bit or 64-bit)
   - Internet Explorer 7 or 8 (IE 6.0 minimum)


User Account Control (UAC) -- Due to continued reports of problems with Solid Edge installation and removal, Solid Edge licensing, Insight web parts and other cases writing to text files in the program folder, it is recommended that the UAC be turned off when running on Windows 7 or Vista.  

        Windows 7: Control Panel -> User Accounts -> Change User Account Control settings ->
                   Never notify

        Vista:  Control Panel -> User Accounts and Family Safety -> User Accounts ->
                Turn User Account Control Off.

--------------------
End of Release Notes
--------------------

-------------------
Installation Notes:
-------------------

After downloading the Maintenance Pack to your machine, dbl click the downloaded
file and the Maintenance Pack will install.

-------------------
End of Installation
-------------------

--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------

=====Assembly=====

PR 6414800: Many times when you push the DELETE on the keyboard the selected object will not delete
PR 6419162: Part cannot be placed in assembly
PR 1787825: Editing failed relationships causes an abort
PR 6400068: Assembly feature cutout results in a warning while in the command
PR 6414695: Crash while in the Assembly explode environment
PR 1797621: Standard Part properties are not correctly transferred to Solid Edge
PR 1803424: Fix made based on submitted Crashlog
PR 2130783: problem in gear accuracy
PR 6401140: Frequent aborts after upgrading to ST2 from v20

=====Draft=====

PR-1805938: Wrong position of Part List in SE ST2 for drawing files created in SEv20
PR 2154348: Updating a drawing view results in a memory error
PR 1804408: Aborting while creating a revolved protrusion
PR 1804916: Angular dimension from create3D causes a crash when retrieved
PR 1805209: Solid Edge aborts when a user drags symbols or blocks into Draft
PR 1807348: Parts list is deleted when a quick sheet template is created

===Insight/View & Markup===

PR 6353576: Rev Mgr set path takes minutes to open folders on Windows 7

=====Part/Profile/Sheet Metal=====

PR 6255537: Changing Datum Reference terminator to a line causes the DR to move with rotate
PR 6258876: Dimension does not behave as expected in synchronous sheet metal file
PR 6414458: Part disappearing from pathfinder when moving a face in assembly
PR 6409937: File Save causes an abort with these two files
PR 1805485: Occurrences are not unsuppressed when removing a region in a 2d profile pattern.
PR 6275277: Failure moving face on CF with circle cutout closed corners

===== Solid Edge Embedded Client=====

PR 1795522: Wrong types of Item object created for SE datasets
PR 1800220: Extremely long open time after Migration from V20 / WSS2 to ST2 / WSS3
PR 1807349: Empty JT-file in TcX-Viewer
PR 6423172: Cannot edit child first time after replacing in assembly structure
PR 6414597: When you In-Place-Edit a component it will be READONLY
PR 6354328: Data Prep - Analyze Errors on Part Linked to Excel file
PR 6411449: Files remain checked out after AddToTeamcenter


---
End
---