Solid Edge ST7 SDK
Solid Edge ST2 MP2 - Readme

--------------
Legal Notices
--------------
©2010 Siemens Product Lifecycle Management Software Inc.

All Rights Reserved
Software, file formats, and audiovisual displays may be used pursuant to the
applicable Software License Agreement and contain confidential and proprietary
information of Siemens Product Lifecycle Management Software Inc.; which is
protected by copyright and trade secret law. Such materials may not be reproduced
or transferred to other documents or used or disclosed to others for manufacturing
or for any other purpose except as specifically authorized within the terms of the
Software License Agreement, or as specifically authorized in writing by Siemens
Product Lifecycle Management Software Inc.

Siemens Product Lifecycle Management Software Inc.
5800 Granite Parkway
Suite 600
Plano, TX. 75024


--------------------
End of Legal Notices
--------------------

--------------
Release Notes:
--------------

Product:        Solid Edge
Version:        102.00.02.06
Date:           04-Jan-2010

This release of Solid Edge has been certified to run on the following:

   - Windows XP Professional© operating system (32-bit or 64-bit)
   - Windows Vista Business© or Vista Enterprise© operating system (32-bit or 64-bit)
   - Windows 7 Professional© or Ultimate© operating system (32-bit or 64-bit)
   - Internet Explorer 7 or 8 (IE 6.0 minimum)

Maintenance Packs are all inclusive and can be installed on top of the base
release or any released Maintenance Pack.

This Maintenance Pack can be installed on top of Versions:
102.00.00.116 or 102.00.01.04


--------------------
End of Release Notes
--------------------

-------------------
Installation Notes:
-------------------

After downloading the Maintenance Pack to your machine, dbl click the downloaded
file and the Maintenance Pack will install.

-------------------
End of Installation
-------------------

--------------------------------------------------
This Maintenance Pack addresses the following PRs:
--------------------------------------------------

=====Part/Profile/Sheet Metal=====

PR 2129581: Japanese JT file name is garbled in PF in V&M
PR 6179945: Unable to add draft
PR 6204548: Bend relief does not update when moving an adjacent thickness face
PR 6206765: Face move fails after specific distance
PR 6211574: After rotating a thickness faces you cannot rotate the layer face
PR 6223877: Move face precedence option resets to default if changed before move initiated
PR 6224744: Cannot change thread size of patterned threads
PR 6227329: Undo of a modify protrusion is causing the file to close
PR 6228094: Unable to move feature origin of pattern along X-axis with a dimension
PR 6247531: Error message displayed when in 2-bend Corner cmd and hitting undo
PR 6248923: Un-checking relation on Advanced Live Rules does not work the first time
PR 6250053: Cannot flatten a converted Sheet Metal part
PR 6250517: Save as Flat creates multiple collinear lines for edges of sync sheet metal part
PR 6251758: Error message displayed attempt to edit bend radius of Contour Flange
PR 6257049: Cannot move a contour flange after rotation
PR 6259575: Can no longer change length of Sync Sheet Metal flange after cutout
PR 6211426: A small piece of round is displayed when editing a flange on this part
PR 6222018: Cannot graphically select a part, not showing on QuickPick menu either
PR 6223164: 2D dims are no longer related after they are migrated to 3D in Synchronous Sheet Metal
PR 6224845: Unable to convert the provided Part file to Synchronous Sheet Metal
PR 6230907: Detached Hole removed from the model after executing Separate command
PR 6249138: Un-checking found relationship on Advanced Live Rules dialog is not remembered
PR 6251813: Simulation never finishes meshing the provided part
PR 6256298: Contour flange rotate fails with all faces in select set
PR 6256312: Rotating base causes Contour Flange thickness face to become non-parallel.
PR 6256448: Some dimensions become sick after attaching a dimple
PR 6256996: Pattern shows occurrence errors if cutout added to pattern
PR 6257012: Cannot move the entire body if there is a locked dimension
PR 6258232: Mirrored partial flange is not attaching
PR 6258248: Live Rules behavior inconsistent for move thickness face
PR 6258809: Thickness chains on adjacent Contour Flanges are not holding together
PR 6258927: Mirroring holes creates asymmetric holes
PR 6259185: Solid Edge aborts when placing a hem along chained edge in specific file
PR 6259992: Ungroup should not be available on the Contour Flange node
PR 6260577: Mirror works sometimes, fails sometimes
PR 6260592: Moving a hole occurrence moves entire pattern, Synchronous Part
PR 6260618: Bend attributes are not copied/pasted
PR 1757612: Menu Groups added to the QAT will not stay there after adding it
PR 1757659: Divide Part does not support rename of the split child anymore
PR 1759155: Results from Simulation not saved if regional settings use a comma delimiter
PR 1759335: A material assigned in Part does not get created in VS+
PR 6196233: Relate fails with Closed Corner on the face being related
PR 6215188: Extent direction arrow does not get repositioned after the feature is repositioned
PR 6221177: Failure moving a Hem
PR 6248058: The result of a Normal Cut is different between V20 and ST2
PR 6248868: Incorrect result when modifying a closed corner
PR 6254474: Unable to set shortcut to specific view orientations
PR 6256344: Rotating semi-circle flange in either direction results in a non-normal to layer face
PR 6256982: Failure moving a face with locked angular dimension
PR 6257097: Failure moving design body when Contour Flange present in model
PR 6258358: Dim handle does not display after selecting lock
PR 6259013: Cannot make the Circle cutout on Contour Flange corner lager then 4 mm
PR 6259911: Continue to get a placement error for command session after first hole failure
PR 6260504: This mirrored flange doesn't attach
PR 6260639: Delete fails when deleting internal flange
PR 6260882: Mirror of a flange fails if layer face of flange selected
PR 6261260: Solid Edge crashes when adding a hole to a pattern
PR 6261301: Etch layer missing on Options dialog for Save as Flat DXF
PR 6261368: Bend properties are not retrieved in Synchronous flat pattern environment
PR 6261494: Unable to move a face of the part
PR 6261997: Pattern will not compute after edit without doing a Recompute every time
PR 6262080: Switching directions or unlocking dimension causes part to change to old value
PR 6262886: After creating a Jog, the dimension does not rebind correctly
PR 6263249: Performance issue changing PMI Font size
PR 6264035: Editing a dimension causes a face to move in opposite direction
PR 6264602: Pattern occurrences are being placed on PF edges, pattern in bad state
PR 6264829: System locks up creating a dimple
PR 6264838: No dimple created error message, but there is a good preview
PR 6264858: Locating 'tab' is allowed in Simulation Express in Synchronous Sheet metal.
PR 6265354:  Provided Synchronous Sheet Metal files won't open
PR 6265472: Mirroring a Hem fails (does not attach)
PR 6266151: Pattern is not removing all occurrences when pattern updates
PR 6266932: Mirror fails with gussets in select set
PR 1762127: Sweep feature fails to recompute
PR 6185234: Patterns/Mirrors don't work correctly with Synchronous Sheet Metal Bend/Jog
PR 6205178: Relate fails to make thickness face coincident to Layer face on Contour Flange
PR 6208142: Moving a Hem is moving the entire tab
PR 6223189: Dimension on Contour Flange fails, move succeeds. Dim edit will succeed if ortho lock off
PR 6223848: Moving group of faces fails with thickness faces on
PR 6246910: Some feature origins are not moving with detached dimples
PR 6258954: Moving a sketch fails with an error
PR 6259025: When the 2nd and 3rd Contour Flanges are moved the widths do not remain constant
PR 6261635: The synchronous flat pattern pane is not displaying after creating a flat pattern
PR 6262187: Editing an angular dimension causes a flange to flip direction
PR 6264724: Can't change the material thickness of a transformed part
PR 6266099: Can't move two flanges
PR 6266261: Can't change corner to closed unless you delete the break corner
PR 6267815: Unable to delete the helix in this part
PR 6268312: Load value does not work the first time entered
PR 6268481: Cannot move a face in this file; no problem moving a similar coplanar face
PR 6268991: Detaching and then re-attaching a break corner looses the break corner definition
PR 6269093: After a face move the formula driven dimension is wrong
PR 6269313: Cannot delete Draft on this part
PR 6269839: Detach mirrored features and then undo causes problems on mirrored feature
PR 6271722: The feature origin for a hole is placed incorrectly with this workflow
PR 6272468: Unable to attach a pattern of flanges after detach
PR 6272515: Deleted pattern occurrence is not shown as suppressed during edit of suppression
PR 1760184:  Draft face analysis is grayed out in Solid Edge Foundation - synchronous
PR 6274676: Flat pattern causes SE to abort
PR 6210632: Dimension to Live Section Edge rebinds to wrong edge
PR 6272437: Pattern fails to create, leaves phantom objects in PathFinder, no Undo
PR 6272944: No move handle if flange pattern occurrence is selected
PR 6274702: Missing flanges on multiple thickness face select for flange creation
PR 6275465: Cannot move thickness faces on CF - Ends and bottom faces
PR 6277934: Moving thickness face fails the 2nd time

=====Assembly=====

PR 6183927: Reports run from Explorer or V&M missing some part nos. and descriptions
PR 6227352: Improvements in fence selection and the Move/Rotate command in synchronous assemblies
PR 6238380: Unable to open a top-level assembly
PR 6246650: Getting an error that the part is a feature library
PR 6247615: Continue to crash working with ERA-Rendering environment
PR 2131442: All surfaces in all the provided part do not show when NX assembly is opened
PR 2133252: ST MP10 aborts while trying to import an assembly from NX3.0
PR 6146834: Solid Edge crashing when attempting to place fasteners
PR 6220404: Import of XT file using an ST assembly template hangs on import
PR 6242272: poor performance when two sketches are in assembly
PR 1757927: Spur gear result is the same with different Unit Correction values
PR 6206843: Peer locate toggle affects synchronous sketch peer locate
PR 6265168: Engineering Reference part edit deletes parts
PR 2134431: Problems changing properties in PROPERTY MANAGER
PR 6249561: Command Ribbon does not honor Japanese font size
PR 6268421:  Simulation study with weldment cannot be meshed
PR 1755806: Part is causing assembly to always save
PR 6053870: Unable to open specific Catia V5 part in Solid edge
PR 6273655: Changes to parts are lost when they are automatically inactivated

=====Draft=====

PR 1689627: property text material property is not showing last known good when file is missing
PR 1747207: symmetric diameter dimensions do not migrate
PR 1752285: Solid Edge crashes in Convert To Geometry
PR 1755410: Solid Edge crashes when opening properties dialog for parts list template
PR 1755493: DXF-export and wrong result
PR 17555536: Unable to set transparent color when inserting image
PR 6250546: Parts list is not sorting mixed numeric and alphabetic columns correctly
PR 6250988: Detail View caption moves to original location during file open
PR 6251907: Attach Dimension command does not locate key-points
PR 6255313: Part list not converting properly to ST2. Items are renumbering w/out updating
PR 6224594: Select all is not selecting cutting plane lines
PR 2124797: Dimension changes between V17 and V20
PR 2134324: Parts list / property text is not handling part weldments correctly
PR 6260815: unable to open some existing draft files
PR 6261564: Callout with custom property "Quantity" is not displaying
PR 1753646: Solid Edge aborts after entering invalid characters on the table style line type page
PR 1760167: Parts list can't be created after copy and pasted of drawing view
PR 1760971: AutoCAD-Layer name definition is ignored
PR 2132106: Creation of a break line will change the value of a dimension automatically
PR 2135361: a phantom sheet is showing up in this file
PR 6247751: Cutting plane terminators printing too thin
PR 6266794: User table is losing line feeds when opened
PR 2124797: Dimension changes when file is opened

===API===

PR 2133734: In SynchronousParts, "objFeature.Faces" cannot be acquired
PR 6268536: SEReader fails to open Assembly locked by Solid Edge
PR 1758666: DetailEditSelectAllInView does not work with Start Command API
PR 1759187: API: Parts List.CopyToClipboard method fails
PR 6272116: overwrite detected when 3dConexion add-in is running

===Insight/View & Markup===

PR 6258121: License error is displayed when opening from V&M
PR 2129578: V&M crashes if open properties dialog box of JT named in Japanese
PR 1753397: Create Full text index is failing
PR 6260575: Default values are not picked up from SharePoint for Solid Edge properties
PR 1759457: Copy alternate assemblies inherits wrong member
PR 6270672: Solid Edge crashes if closing Search dialog before list refreshes
PR 6270698: Solid Edge crashes if you click Search before old list is processed

=====Embedded Client=====

PR 6184631: SEEC open dialog is not opening according to variant rule
PR 1754089: Assembly structure links are broken with "Hide all Components"
PR 6258900: custom property specifying Item Type is incorrect
PR 1734817: Sequence Number won´t update during open of assembly
PR 1754460: SEEC does not synchronize PSE BOM although "SEEC_BOM_Synchronize=TRUE"
PR 6244979: SEEC does not update the precise BOM
PR 6253200: Light weight data leads to 0.000000 Mass Property
PR 6272401: Delivered the new set of data prep utilities

---
End
---